The remote access feature allows your data logger to call home to our factory. This is a secure, encrypted tunnel between your logger and our tech support team to access the device to assist someone who is troubleshooting a situation and would like additional guidance from us.
Note: This is not intended to replace the person responsible for on site field configuration/programming and commissioning of the product. It also is not intended to replace initial troubleshooting that should be performed first by the owner of the system.
For everyone's security, we do not maintain your log in information for our customers devices, and we will need to be provided your login credentials to the device for every support session, just as anyone accessing the device on site would be required to have available.
Below will detail the different methods on how you can enable the feature depending on the device model #.
Enabling the Remote Access feature on your datalogger while logged into its web interface-
Enabling the Remote Access feature on your datalogger from the LCD-
** Examples what these devices look like can be found in this article here.
After enabling the RA feature, watch the LCD or the web interface for the connection status.
It may take 5 minutes and you may see ‘RA blocked’ appear several times.
It will show “R-A Connected” then display a “SN” and “R-A pin” when it connects successfully. Please record both and provide them to the agent you are working with.
Should that not work, it may then be best to involve someone who manages the LAN to help check the internet connectivity from that LAN cable with a PC. In business and corporate LAN settings your IT teams may have additional security features where port 2022/tcp outbound may need to be unblocked.
Note: This is not intended to replace the person responsible for on site field configuration/programming and commissioning of the product. It also is not intended to replace initial troubleshooting that should be performed first by the owner of the system.
For everyone's security, we do not maintain your log in information for our customers devices, and we will need to be provided your login credentials to the device for every support session, just as anyone accessing the device on site would be required to have available.
Below will detail the different methods on how you can enable the feature depending on the device model #.
Enabling the Remote Access feature on your datalogger while logged into its web interface-
A7810, A8810, A8812, A8814: | EMHXD: |
Networking > Setup > “Allow Remote Access” | Networking > Remote Access > “Allow Remote Access” |
Enabling the Remote Access feature on your datalogger from the LCD-
A7810, A8810, A8812: | A8814: | EMHXD: |
Use the "Menu" and "Select" buttons to locate the following: Main Menu -> TCP/IP Config > "R-Access on/off" | Use the touchscreen to navigate from the home screen to: Network > Allow Remote Access | Use the five buttons to navigate the menu tree to locate: Full Setup > Network > Remote Access > Enable/Disable. Once enabled, select Show Status. |
After enabling the RA feature, watch the LCD or the web interface for the connection status.
It may take 5 minutes and you may see ‘RA blocked’ appear several times.
It will show “R-A Connected” then display a “SN” and “R-A pin” when it connects successfully. Please record both and provide them to the agent you are working with.
Should that not work, it may then be best to involve someone who manages the LAN to help check the internet connectivity from that LAN cable with a PC. In business and corporate LAN settings your IT teams may have additional security features where port 2022/tcp outbound may need to be unblocked.
Last edited: