The Leviton Energy Monitoring Hub datalogger by default typically needs the following ports enabled for inbound or outbound traffic.
Additional ports may be required depending on the configuration options set in the device. For example, Modbus TCP or BACnet IP communications.
If the appropriate ports are open yet there are still connectivity issues, it may be worth revisiting the physical connectivity and the LAN settings at the EMH.
| Port (default) | Direction | Description |
| 80/tcp 443/tcp | inbound |
|
| 80/tcp 443/tcp | outbound |
|
| 37/tcp 123/udp | outbound |
|
| 53 | outbound |
|
| 2022/tcp | outbound |
|
| 21/tcp | outbound |
|
| 1024-65535/tcp | outbound |
|
| 20/tcp | inbound |
|
Additional ports may be required depending on the configuration options set in the device. For example, Modbus TCP or BACnet IP communications.
If the appropriate ports are open yet there are still connectivity issues, it may be worth revisiting the physical connectivity and the LAN settings at the EMH.
Last edited: