Setting your EMH to upload data to BMO
Begin by logging into your EMH using a web browser on your PC. Your PC can be connected to the EMH if they are both connected to the same LAN. While it may be easier to connect to it with a direct LAN cable, you will not be able to test the data upload from the EMH to BMO with that method.If you successfully reach the EMH web interface, proceed in clicking on the link or button to log in.
The username will always be ‘admin’. The password is typically set to ‘admin’.
Upon successful login, use the left side menu options to browse to the following (depending on your product model):
| A7810/A8810/A8812/A8814 | EMHXD/EMHSP |
| Devices > Devices List | Devices |
Please check that all expected devices are listed on the screen, are named, and are status OK before proceeding further.
Now, browse to the following menu location:
| A7810/A8810/A8812/A8814 | EMHXD/EMHSP |
| Log File Data > Setup / Upload | Uploads |
In this location, we typically recommend setting your scheduled upload time to “connect every 15 minutes”.
Next, locate an available upload channel and configure it to the following-
Protocol:
| A7810/A8810/A8812/A8814 | EMHXD/EMHSP |
| Obvius Building Manager Online with SSL/TLS Security | BMO with TLS Security (specify URL) |
URL: https://upload.levitonbmo.com/
Set an upload password of your choosing and note the serial number of your EMH. Record these items in a safe and recoverable place as they will be needed later. to locate the serial number of your EMH, this is located:
| A7810/A8810/A8812/A8814 | EMHXD/EMHSP |
| At the top of the Log File Data > Setup / Upload screen | The upper right corner of your screen in the header |
Now click “Apply”.
If internet connectivity to the EMH is available, you may click the Upload Data Now button to allow the logger to attempt its first synchronization with the BMO cloud servers.
If you have any uncertainty regarding the internet connectivity, please run the connection test first.
Run a connection test to BMO
Browse to the following location:
| A7810/A8810/A8812/A8814 | EMHXD/EMHSP |
| Testing / Diags > Connection Test | Diagnostics |
Click “Begin Test”. It should take about 30 seconds to complete.
You will want to confirm a success message for the upload channel configured to BMO. Otherwise, the diagnostics from that test may be useful for whomever manages your LAN to investigate further.
Please refer to the following article regarding LAN connectivity for your EMH, then after any necessary adjustments, try the connection test again to confirm functionality.
Force data uploads to make the logged data readily available
Self registration at levitonbmo.com requires the EMH successfully having communicated at least twice to the levitonbmo.com servers. If you don't want to wait for the scheduled upload times set earlier, you may force upload sessions by heading to the following location:| A7810/A8810/A8812/A8814 | EMHXD/EMHSP |
| Log File Data > Setup / Upload > Upload Data Now | Uploads > Upload Data Now |
At the top of the screen, there will be a status bar. A scheduled date and time indicates no upload is in session. Press the button and the status will change indicating progress, eventually ending at a future scheduled date and time. Complete two sessions, and then proceed to levitonbmo.com to register your new account or import this EMH to your existing one.
Last edited: