Various submeter manufacturers utilize different conventions when referring to energy consumption, generation, and power (demand). The following table is to provide a reference of the same datapoint types across our diverse line of metering products.
CT orientation and phasing to the voltage must be correct for the meter to register usage accurately. Otherwise energy counters may accumulate in the opposite direction expected.
* Not applicable - product is a uni-directional measurement device
** Datapoint is only available when used with or communicated through a Leviton Energy Monitoring Hub. Please reach out to technical support for more information.
*** Due to the flexibility of maximizing meter inputs to this meter, there aren't separate datapoints for this. The meter reports one kWh datapoint, the Element Net Sum, which is Imported Energy - Exported Energy.
| Series 3500 | Series 4000 | Series 4100 | Series 6000 | Series 7000/7100 | Series 7200/7300 | Series 8000 | |
| Energy delivered from the utility/grid to be consumed by a load engineering unit of kWh | kWh from grid | Real Energy Consumption | Real Energy Quadrants 1 & 4, Import | Positive active Energy : Ea+ | Imported Energy Sum | (see note) *** | Energy Delivered |
| Per phase delivered from the utility/grid to be consumed by a load Useful for ASHRAE / IECC disaggregation of loads applications engineering unit of kWh | N/A | N/A | Accumulated Real Energy, Phase X, Import | N/A | Imported Energy CH# | < Combine circuits in virtual elements in meter programming > | < Configure meter in 1P-## mode > |
| Energy being generated on site feeding back towards the grid/utility engineering unit of kWh | (N/A) * | (N/A) * | Real Energy Quadrants 2 & 3, Export | Total Negative active Energy : Ea- | Exported Energy Sum | (See note) *** | Energy Received |
| Present (Average) Demand engineering unit of kW | Present Demand ** | Total Real Power Present Demand | Total Real Power Present Demand | (Refer to Series 6000 Modbus Map for more info.) | Power Demand This Interval -or- Watt Demand Element | Element Demand Now | Present Demand |
CT orientation and phasing to the voltage must be correct for the meter to register usage accurately. Otherwise energy counters may accumulate in the opposite direction expected.
* Not applicable - product is a uni-directional measurement device
** Datapoint is only available when used with or communicated through a Leviton Energy Monitoring Hub. Please reach out to technical support for more information.
*** Due to the flexibility of maximizing meter inputs to this meter, there aren't separate datapoints for this. The meter reports one kWh datapoint, the Element Net Sum, which is Imported Energy - Exported Energy.
Last edited: