The Series 2000 meter with demand will rotate 4 different values on the LCD.
For more details, please refer to the manual of your Series 2000 meter.
Additional credit to Sam Moran for this article
| All 8's appear on the LCD | this is a test screen to demonstrate all segments of the LCD are functioning |
| No dots on the bottom of the LCD | Energy consumption appears in kWh. This register counts upwards, just like the odometer in a car for distance traveled. This value cannot be reset. |
| Dot appears next to Instantaneous Demand | Last 5 minute average demand (power) in 1/100 of a kW (Example photo shows 15.42 kW) |
| Dot appears next to Peak Demand | Peak demand based on a 15 minute rolling demand interval, in 1/100 of a kW (Example photo shows 40.56 kW) |
For more details, please refer to the manual of your Series 2000 meter.
Additional credit to Sam Moran for this article
Last edited: