Password and factory resets

This article discusses admin login password reset and factory reset options from the LCD and push buttons on the A7810, A8810, and A8812 Leviton Energy Monitoring Hub dataloggers.
This covers:
  • Password default configuration
  • Password reset instructions
  • Factory reset instructions

Password default configuration

Prior to 2020, the default login username is admin, and the typical default password from our factories were 'admin', 'leviton', or 'password'.
As of 2020, we no longer ship the device with a factory set password to comply with California Law SB-327 that enhances security for anyone utilizing network connected devices. As such, a user must set the password on first login to the device. On that same configuration screen, the user also configures whether the password can be reset using the LCD and push buttons on the device.

When sold, configured, or managed by a third party, they may have been set with a different shipping default.


Password Reset Instructions

You will only be able to locate this setting in the menu if the device is running v02.20.0122 firmware or greater. The version of the firmware appears on the LCD as one of the messages after the reboot.

The feature must have also been enabled in configuration. If a device was upgraded to newer firmware support this feature, it is defaulted to being off to maintain security. Someone logged in as admin to the web interface of the device can edit the setting under Security > Admin.


Steps:
Begin these steps on the home screen. Locate the Menu and Select buttons on the product.
To ensure you're on the home screen, click the Menu button until you see the option "(previous menu)", then press the Select button. If you still see at the top bar some text between brackets eg. "[Main Menu]" after performing this, repeat these steps until you don't see this.

1. Simultaneously press and hold the Menu and Select buttons until the [Advanced Menu] appears.
2. Press the Menu button until the “Reset password” option appears.
-- [Did you reach “(previous menu)” first? If so, the feature is disabled or not available. Stop.]
3. Press the select button.
4. Display reads “Reset Admin password” and then “Confirm Reset? Menu=N Select=Y”.
5. Prepare your phone camera or some method to jot down the secure password.
6. Press the select button for yes.
7. Use temporary password to access the unit.
8. Navigate to Security > Admin to “Change Password”.

Note: There are certain versions of firmware which may inadvertently display the "reset admin password" option in the Advanced Menu even though it was never originally enabled. If when selecting it, the password does not appear, then the feature was not enabled. As such, that confirms that the setting was not activated in programming and the EMH is continuing to provide the appropriate level of security for the device.

If password reset was not available, the last resort method to log into the device will be to factory reset the logger. Someone will need to reprogram the unit completely to restore the device to its previous fully working state.

If a Leviton field service tech previously assisted with the programming of your device, it is possible to purchase their services to have them return to site to help with reprogramming.


Factory Reset Instructions

Below, please start on step 2 if you followed the password reset instructions above and stopped with “(previous menu)” displayed.

1. Simultaneously press and hold the Menu and Select buttons until the [Advanced Menu] appears.
2. Press the Menu button until "Erase log/config" option appears.
3. Press the Select button.
4. Display reads "This will erase all settings!" and then "Clear Disk? Menu=N Select=Y".
5. Press the Select button for yes. You may not see the LCD screen indicate anything for a minute.
6. Display will eventually read "Reboot required Press "select"". Do So.
8. Display reads "Reboot requested Please wait..." then "Rebooting Please wait..."
9. After reboot the unit will be accessible with the default password or be prompted to set a new password. Note that the IP address may have changed.
 
Last edited:
Back
Top