I installed the configuration utility for the S7000. But the CT selector box is empty.

There are TWO configuration utilities, one for the series 7000/7100 and one for the series 7200/7300
The CT pictures and data are stored in a file named "Local" The folder must be located in the local drive root directory.


The one for the series 7000/7100 is called "Power Meter Viewer."
C:\Power Meter Viewer\Local​

The one for the series 7200/7300 is called "Virtual Element Viewer."
C:\Virtual Element Viewer\Local​
 

Attachments

  • Local.zip
    462.8 KB · Views: 2
Last edited:
Back
Top