A DRC application requires a ceiling mount occupancy sensor mounted at 25' above finished floor. Has the the OSR15-MCW been mounted at 25' mounting heights on previous applications. Astatically it fits the application well.
Can the DRKDN-U4W be programed to return to full light on? The requested sequence of operation is. ZSC04-INW set with 10 minute time delay , after no presence is detected the lights dim to 50% for one minute. If the occupant moves within the space during the one minute partial off, the sensor...
Low voltage room control with emergency power application. 1 x DRC00-0L0 room control communicating with 2 x DRDDP-A40 in an application. The DRC00-0L0 is connected to emergency power source through the EM panel. When the generator is cycle tested the dimmed phase loads do not return to the most...
I have a project with both lighting and controlled receptacles in the same room. The sensors are setup as vacancy sensors meaning the room is in manual on and user must push a button to turn on the lights. The receptacles are off even though the room is still occupied. How do I fix this...
Low voltage room control with emergency power application. 1 x DRC00-0L0 room control communicating with 2 x DRDDP-A40 in a application. The DRC00-0L0 is connected to emergency power source through the EM panel. When the generator is cycle tested the dimmed phase loads do not return to the most...
This site uses cookies to help personalise content, tailor your experience and to keep you logged in if you register.
By continuing to use this site, you are consenting to our use of cookies.