Recent content by Aaron Lang

  1. Aaron Lang

    maximum fade rate available in Sapphire

    6512 seconds. 108 minutes, or 1.8 hours. Anecdotally gleaned from conversation with A. Maples.
  2. Aaron Lang

    maximum fade rate available in Sapphire

    What is the maximum fade rate available in Sapphire?
  3. Aaron Lang

    GreenMAX relay panel Room Combine

    What are the requirements for GreenMAX room combine? We understand that KCLCM and NPG LN are needed. Which controls need to be in the rooms to be combined? Will GreenMAX button stations suffice? Is a Sapphire needed? Is a Sapphire required in each room to be combined?
  4. Aaron Lang

    ZS057-D0Z 3-way operation

    Thank you! Wondering too what '3-way switching' is intended to convey on datasheet.
  5. Aaron Lang

    ZS057-D0Z 3-way operation

    Datasheet for this product lists "3-way switching" as a feature. To be clear, does the product operate in a 3-way configuration with itself for 3-way dimming?
  6. Aaron Lang

    Guideline for sapphire screen setup

    What is the maximum number of buttons and sliders on a Sapphire page? I have heard rumor that the maximum number of buttons is 16 and max number of sliders is 12.
  7. Aaron Lang

    DRID0-C02 & OSC10-M0W

    The OSC10-M0W sensor has its own function parameters that are physically set at the device; the DRC app would have no way to access those parameters. See installation instructions for those settings: OSC10-M0W installation sheet
  8. Aaron Lang

    PST24-I10

    Hi. We have several large high profile jobs that are waiting on confirmation of this.
  9. Aaron Lang

    PST24-I10

    What is the power input rating of this device? Application for up to 277V? Concerned because there are discrepancies in literature.
  10. Aaron Lang

    ODD24-IDW

    Can ODD24-IDW be used in conjunction with a power pack and other sensors like ceiling and wall mount units?
  11. Aaron Lang

    Sapphire, button stations, and DMX fixtures

    When using a Sapphire with DRKDN-CxW button stations and DMX fixtures controlled through an NP00G, can the button stations be used to access Scene buttons on the Sapphire.
  12. Aaron Lang

    LU04P

    The data sheet for this item says 'Phase Cut Dimming Power Pack (LU04P) allows for dimming of full phase loads' but does not go into any detail about forward or reverse phase. Please clarify load types suited to this unit.
  13. Aaron Lang

    Wireless DRC 1-button room controller DRKDN-U1W dimming feature

    Can wireless DRC 1-button room controller DRKDN-U1W can be programmed for dimming? I've seen "press and hold" dimming in other LEV products. Can this product do that? This document seems to indicate such...
  14. Aaron Lang

    Automatic System Configuration

    Please define the preset parameters 1-4 on the 8 button station.
Back
Top