The remote access feature allows your data logger to call home to our factory. This is a secure, encrypted tunnel between your logger and our tech support team to access the device to assist someone who is troubleshooting a situation and would like additional guidance from us.
Note: This is not intended to replace the person responsible for on site field configuration/programming and commissioning of the product. It also is not intended to replace initial troubleshooting that should be performed first by the owner of the system.
For everyone's security, we do not maintain your log in information for our customers devices, and we will need to be provided your login credentials to the device for every support session, just as anyone accessing the device on site would be required to have available.
Below will detail the different methods on how you can enable the feature depending on the device model #.
** Examples what these devices look like can be found in this article here.
When disabling, the feature will disconnect right away.
After enabling the RA feature, watch the LCD or the web interface for the connection status. It may take up to 5 minutes and you may see ‘RA blocked’ appear several times.
As soon as you see “R-A Connected” then display a “SN” and “R-A pin” when it connects successfully. Please record both and provide them to the agent you are working with.
Should that not work after the elapsed time, it may then be best to involve someone who manages the LAN to help check the internet connectivity from that LAN cable with a PC. In business and corporate LAN settings your IT teams may have additional security features where port 2022/tcp outbound may need to be unblocked.
RA connections from EMHs in the field today may be set to "sleep" by our servers after being inactive for 30 days. When sleeping, it will wake every 24 hours to check back in for a flag that tells it to become a fully continuous active connection again. This can be overridden by turning the RA connection off and back on at the device, but if someone is on site to do this, it would be recommended to have them verify more items relating to the network connectivity of the device.
Note: This is not intended to replace the person responsible for on site field configuration/programming and commissioning of the product. It also is not intended to replace initial troubleshooting that should be performed first by the owner of the system.
For everyone's security, we do not maintain your log in information for our customers devices, and we will need to be provided your login credentials to the device for every support session, just as anyone accessing the device on site would be required to have available.
Below will detail the different methods on how you can enable the feature depending on the device model #.
Enabling the Remote Access feature on your datalogger while logged into its web interface-
| A7810, A8810, A8812, A8814: | EMHXD, EMHSP: |
| Networking > Setup > “Allow Remote Access” | Networking > Remote Access > “Allow Remote Access” |
Enabling the Remote Access feature on your datalogger physically at the device from the LCD-
| A7810, A8810, A8812: | A8814: | EMHXD, EMHSP: |
| Use the "Menu" and "Select" buttons to locate the following: Main Menu -> TCP/IP Config > "R-Access on/off" | Use the touchscreen to navigate from the home screen to: Network > Allow Remote Access | Use the five buttons to navigate the menu tree to locate: Full Setup > Network > Remote Access > Enable/Disable. Once enabled, select Show Status. |
Notes on what to expect when utilizing this feature
When disabling, the feature will disconnect right away.
After enabling the RA feature, watch the LCD or the web interface for the connection status. It may take up to 5 minutes and you may see ‘RA blocked’ appear several times.
As soon as you see “R-A Connected” then display a “SN” and “R-A pin” when it connects successfully. Please record both and provide them to the agent you are working with.
Should that not work after the elapsed time, it may then be best to involve someone who manages the LAN to help check the internet connectivity from that LAN cable with a PC. In business and corporate LAN settings your IT teams may have additional security features where port 2022/tcp outbound may need to be unblocked.
RA connections from EMHs in the field today may be set to "sleep" by our servers after being inactive for 30 days. When sleeping, it will wake every 24 hours to check back in for a flag that tells it to become a fully continuous active connection again. This can be overridden by turning the RA connection off and back on at the device, but if someone is on site to do this, it would be recommended to have them verify more items relating to the network connectivity of the device.
Last edited: