Recent content by reidparks

  1. R

    CSI Division 26 Specification for Occupancy Sensors

    https://leviton.com/products/commercial/lighting-controls/occupancy-sensors-and-vacancy-sensors/smart-sensors Use web address above to see latest Smart Sensor product offering.
  2. R

    Installing OSSMT-GDX in hazardous storage areas

    OSSMT is not rated for hazardous storage areas.
  3. R

    Max PLVSW-4LW on O5C20-MDW

    Up to 2x PLVSW devices can be wired to a Provolt PRC, with an additional 4x devices daisy-chained to each of the PLVSWs wired to the PRC (so up to 10 total keypads).
  4. R

    Pro Volt App on newer Androids not avaiable?

    Try again, the app should now be available again for older Android devices.
  5. R

    Time Drift issue in Smart CMS Multi-Tech 0-10V Dimming Models when running schedules

    It was recently discovered that the Smart CMS AC705 and ACY20 models are not keeping time accurately when scheduling is implemented using the Smart Sensor App. This feature is being temporarily removed and will be re-released in the near future when fixed. This issue only occurs with the...
  6. R

    O5C20-MDW Question

    You can wire 2x PLVSWs per O5C20-MDW (or any Provolt sensor), however, you can also daisy-chain up to 4x additional PVLSWs to each of those switches (so technically up to 10 total). Newer Smart CMS Sensors are the same way, however, you can also use the new wireless companion dimmers too (up to...
  7. R

    Provolt

    For Provolt, the models can be mixed somewhat, but we would recommend room controllers (0-10V dimming models) only be used with other room controllers and sensors (switching only) only used with other sensors. When we launch the new Smart Version next month (ie: Provolt +), you will have the...
  8. R

    OSMHB-VDW won't turn on?

    Issue is likely a defective sensor. Please return for a replacement unit. Sorry for the inconvenience.
  9. R

    Provolt

    Yes, multiple PRCs (Room Controllers) or Provolt Sensors can be wired together with multiple PLVSW keypads. Here is a classroom application with with 2x O6Cxx Room Controllers and 2x PLVSW-4LW wallbox stations.
Back
Top