Recent content by sdo

  1. S

    Series 8000 Firmware Updates

    The Series 8000 firmware updater PC application and update file is linked below. Unzip both downloads prior to use. The field firmware update is intended to be performed by trained technicians. Instructions are provided. Use at your own risk, as improper use of the tool may result in an issue...
  2. S

    Current Transformer Paralleling

    Please be aware that Leviton has updated guidance on this topic. The article above should no longer be referenced.
  3. S

    Device comms statistics

    The Devices page of the EMH helps provide ongoing stats on RS485 packets sent, received from the end device, any errors, and response time (round trip time). This can help you determine signal strength or hardwired RS485 issues, optimizing timeout settings, and verify if any changes have helped...
  4. S

    Managing Logins for Your LevitonBMO.com Account

    Managing Logins for Your LevitonBMO.com Account This article explains how to manage logins for a LevitonBMO.com account and outlines the security measures in place to protect user access. LevitonBMO.com is a software service that is a separate layer on top of the Data Acquisition Server(s) that...
  5. S

    Initial BMO Account Setup

    Introduction The following information covers the initial setup of a new account on the levitonbmo.com cloud submetering platform. If you already have a login to levitonbmo.com, you can skip the steps below and import the new Leviton Energy Monitoring Hub (EMH) datalogger using the EMH...
  6. S

    EMHXD EMHSP release candidate firmware v04.26.0413

    We are pleased to provide the latest firmware release candidate v04.26.0413 for the Leviton EMHXD and EMHSP. Links related to this release are provided below for download. Users guide Firmware download link (unzip before use) Sample containers package v04.26.0312 for release candidate...
  7. S

    Series 7000/7100 and 7200/7300 Data Presentation Differences

    For the purposes of this article, we will refer to the 7200/7300 family of meters as the "virtual element" (VE) style meters. Virtual vs. Non-Virtual Meter Elements: What’s the Deal? If you’ve ever tried to integrate a power meter and found yourself knee-deep in Modbus IDs and register maps...
  8. S

    Optimizing Polling Response Latency

    Possible Solution: Optimizing BACnet Polling Performance Slow BACnet polling response (4+ seconds) can be due to several factors related to network setup, register mapping, polling strategy, and firmware configuration. Here's how to tighten that up: 1. Reduce the Number of Polled Registers...
  9. S

    Pulse counting products and their max rate

    Part#Default Counting SpeedAdditional Configuration Options A833210Hz- A8812 I/O10Hz- A781010Hz50, 100Hz A891110Hz50, 100Hz R912010Hz50, 100, 250Hz Pulse signals must be 50% duty cycle at the rated counting speed
  10. S

    Series 7200/7300 Modbus RTU and TCP datapoint listing

    Linked here is the datapoint listing for the 7200/7300 Virtual Element Meter. Please be aware that the datapoint mapping in this meter is a feature enhancement layer built on top of the original 7000/7100 functionality. Refer only to the datapoints listed under sections described in the header...
  11. S

    PhaseChek - Best Practices and Optimizing Results

    Understanding PhaseChek: Best Practices for Reliable Results PhaseChek is a valuable diagnostic tool designed to provide a quick assessment of meter programming and physical installation. While it’s effective at identifying potential issues that warrant further investigation, it’s important to...
  12. S

    Setting up your EMH to upload to LevitonBMO.com

    Setting your EMH to upload data to BMO Begin by logging into your EMH using a web browser on your PC. Your PC can be connected to the EMH if they are both connected to the same LAN. While it may be easier to connect to it with a direct LAN cable, you will not be able to test the data upload from...
  13. S

    Clearing accumulated counts

    Important details Resetting counts requires interfacing with the device using the configuration tool. Physical access to the meter is typically required to initiate this process. Not all meters support count clearing; some versions are sealed or restricted to prevent this functionality. Before...
  14. S

    Understanding Serial Number Encoding from Modbus Registers

    This guide walks through how to interpret the serial number from the device’s Modbus response and explains the conversion process step by step. This article applies to the following part numbers: R9120 A8332 A8911 A90DC A89DC What You Receive from the Device These devices return their serial...
  15. S

    CT wires and extensions best practices

    Please refer to this document linked here for which Leviton CTs can be extended and distance recommendations. This article is to supplement the information in that document to include additional recommendations for best practice. Avoid creating large loops of CT wiring, and limit the amount...
Back
Top