Recent content by dbuerer

  1. dbuerer

    DRC Analog Input Device

    Both great questions. At this point, there is no way to "lock out" sensors and switches via any method other than the scheduler. This feature is however on the development schedule. With respect to using it to create a master switch, this is at present not a supported application . However...
  2. dbuerer

    How do I change my password or other preferences?

    To update your password or other user preferences, start by logging into the system. 1. In this example, i've navigated to myBuilding.Leviton.com and logged in as Silly User. 2. Access the user preferences menu by selecting your Avatar in the upper right hand corner of the window 3. From...
  3. dbuerer

    You're putting what!? in my rack?

    Yup it's true.....our project requirements require us to Install our My Building software product at your facility. What's My Building you say? Check out these helpful articles to learn more about it: 1 2 3 Often, we are supplying My Building software on computer that is shipped to your job...
  4. dbuerer

    Using ODD24-IDW with DRC

    Please see: DRC Analog connection with ODD24-IDW at https://communities.leviton.com/threads/drc-analog-connection-with-odd24-idw.53/#post-103
  5. dbuerer

    Screen changing scenes on its own

    This situation can occur when the electrical ground is excessively noisy. The solution is to isolate the touchscreen from the backbox by using nylon screws and washers to fully isolate the screen from the backbox. This is a simple resolution to the problem of the screen changing on it's own...
  6. dbuerer

    How do we handle room combine with DRC and occupancy sensors?

    Although there are more elegant ways in development to address this, the best way to handle it at this point in time is to use a KCLCM combine closure interface to execute a channel level combine. Any sensors would be connected together in parallel using a smart pack (DRDD7) or multi-channel...
  7. dbuerer

    Installation of My Building at Customer's Site

    This article covers the installation of the My Building software on a customer's computer, physical, or virtualized. The audience is the devops engineer that will be installing the software. You may find it helpful to review the following articles prior to beginning installation which should...
  8. dbuerer

    Communication To & From My Building....What ports must be open?

    My Building communicates between software modules, the network, and other Leviton equipment on the IP network. Most of this communication is TCP/IP communication, however, some of it is UDP/IP. This article document what type of communication is required between various parts of the system...
  9. dbuerer

    My Building Terminology/Definitions

    There are several terms used in these training articles, some of which may be unfamiliar to you. This is a short list of said terms and information about how we use them. Feel free to comment before if you'd like us to add some to the list! the term in the parenthesis following the name is...
  10. dbuerer

    Can GreenMAX Relay Panels be used with My Building?

    This is one of those yes & no questions. First, the yes....GreenMAX Relays themselves can be used with My Building so long as they are first enrolled to a DRC Room Controller. The GreenMAX Relay is enrolled as a "channel" to the DRC Room controller which will give you the ability to assign...
  11. dbuerer

    Virtualization

    Can My Building be installed on a "virtual" sever? Absolutely! It also can be installed on a local physical server if that's more your cup of tea. However, in this article we will be working through the details of what virtualization is, how to achieve it with the My Building software suite...
  12. dbuerer

    Upgrading My Building

    From time to time you may need to update one or more parts of the My Building software. This article walks you through said process. The steps identified herein assume you're running a k8s deployment. If your system is different, the steps will be similar but may have to be custom tailored...
  13. dbuerer

    Connecting DRC to a Wi-Fi Network, DRC Networking Requirements

    Would need more details to answer said question however it's best to work with the site's IT team to ask this question as they would be the owners of the VPN and it's associated rules. All DRC devices, inclusive of the app, use TCP/IP to communicate to the room controller.
  14. dbuerer

    Connecting DRC to a Wi-Fi Network, DRC Networking Requirements

    DNS is only required when you're using dynamic address as the Room Controller and the app uses the "host name" to connect. The Host name is the name of the room. When you use static ip address, the assigned ip address is used to connect.
  15. dbuerer

    Network requirements for GreenMAX

    Thank you for confirming!! That's great. I would not thought of it being a character set issue.
Back
Top