Answer: Industry convention for color coding in 3 Phase 208V electrical systems assigns the color black to phase A, red to phase B, Blue to phase C, and white to Neutral. Leviton‘s 100A and 200A solid core CTs are coded with the same colors (on the body of the CTs and on the wires) to help...
A: Yes. You should try to avoid extending the native CT leads by locating the meter next to the circuit breaker. If you must extend the leads, take into consideration the following inaccuracy contributors. Here are some of the factors that will affect accuracy when using long CT leads:
1. Wire...
Answer: The meter should not be used in this configuration. The per-phase energy, power, voltage and amperage values in this configuration will be correct, however the Line-to-Line voltage will be calculated for a balanced 3phase system, and will not represent the actual L-L voltage. If the...
Answer: Yes. The meter must be installed with the neutral terminal disconnected. Note: Line-to-Neutral voltages will be reported for a virtual neutral. (e.g. L-L=480V, L-N=277)
Answer: The meter should not be used in this configuration. The per-phase energy, power, voltage and amperage values in this configuration will be correct; however the Line-to-Line voltage will be calculated for a 3phase system, and will not represent the actual L-L voltage.
It's a valid question. I think the attached document will help to explain how these CTs work. Following is an excerpt with a summary of the math used with these CTs.
The principle of operation of a CT is the sensing of the magnetomotive force around a current-carrying conductor. The CT...
The Series 6000 split core CTs (CTSxx part#) do use a 333mV output, but they are not interchangeable with our other 333mV CTs. The S6000 meters are designed for use with these custom, auto-ranging CTs and they require an RJ12 connection.
The Rogowski CTs are not 333mV. Most Rogowski CTs...
There are 3 places to find the device ID (serial number):
There is a sticker on the back of the unit, if it hasn't been mounted.
It is displayed on the login screen.
It is also available from the System/Identification tab in the main user interface
This document summarizes the application of a Series 4000/4100 Meters on a three phase, four wire delta service for a cost-effective solution for monitoring multi-phase tenant energy usage.
The purpose of this technical note is to identify specific installation requirements associated with the S8000 Meter platform for 3PH Delta service configurations.
The short answer is yes. However there are a number of secondary considerations. If the loads are in the same vicinty or panel, where the conductors can be grouped together through a single CT, they could be monitored by a single meter. The meter and CT would need to be rated for at least the...
This site uses cookies to help personalise content, tailor your experience and to keep you logged in if you register.
By continuing to use this site, you are consenting to our use of cookies.