Search results

  1. smoran

    Screen changing scenes on its own

    After installation, the Touch Screen seems to be possessed, and it is changing scenes own its own What causes that? How do I fix it?
  2. smoran

    Internal Modbus Registers for the AcquiLite EMB A7810

    The attached PDF has a listing of the internal Modbus registers for the A7810
  3. smoran

    S7200 and S7300 Firmware

    Virtual meter series S7200 and S7300 firmware
  4. smoran

    EzMAX H Key Replacement

    What is the part number for the EzMAX H panel replacement key?
  5. smoran

    LumaCan Sensors and Analog Sensor Controlling the same relay or group

    Can an OSR15-MCW or any other LumaCAN sensor, in conjunction with an analog sensor connected to an AI input? Be assigned to control the same load? If yes, what is the order of operations? Does one take priority? Or Does the first activated sensor turn the load ON, and the last sensor to time...
  6. smoran

    Circuit Breaker Rating

    Are the breakers in the TLLP rated at 100% load or do they need to be derated? For example, if my track load is 10 amps. Do I need to specify a 10Amp breaker in the panel or a higher to include derating? If derating is required. What is the percentage?
  7. smoran

    DALI 2 Compliant

    Is the DALI gateway compliant with DALI2? if not will it still work with DALI 2 and what are the limitations?
  8. smoran

    I installed the configuration utility for the S7000. But the CT selector box is empty.

    There are TWO configuration utilities, one for the series 7000/7100 and one for the series 7200/7300 The CT pictures and data are stored in a file named "Local" The folder must be located in the local drive root directory. The one for the series 7000/7100 is called "Power Meter Viewer."...
  9. smoran

    How to add a user level pin / password

    User-level Pin is assigned on a page basis. this allows the administrator to grant access to pages with different levels of control. If desired the same Pin can be used for every page. From the home page enter the Page Settings Mode. On the bottom center of the screen, press on the Date and...
  10. smoran

    Series 7000 and 7100 master Modbus register list

    Series 7000 and 7100 master Modbus register list
  11. smoran

    Current D4200 Compatibility with old model and remote stations

    Is the current D4200-0LW compatible with a system with a first generation D4200-1LW with a Combine Closure and Remote Stations D42P-RLW?
Back
Top