Search results

  1. smoran

    EzMAX H Key Replacement

    The EzMAX H uses a standard cabinet key number CH751 it can be purchased from any locksmith or Amazon
  2. smoran

    EzMAX H Key Replacement

    What is the part number for the EzMAX H panel replacement key?
  3. smoran

    LumaCan Sensors and Analog Sensor Controlling the same relay or group

    Can an OSR15-MCW or any other LumaCAN sensor, in conjunction with an analog sensor connected to an AI input? Be assigned to control the same load? If yes, what is the order of operations? Does one take priority? Or Does the first activated sensor turn the load ON, and the last sensor to time...
  4. smoran

    Circuit Breaker Rating

    Are the breakers in the TLLP rated at 100% load or do they need to be derated? For example, if my track load is 10 amps. Do I need to specify a 10Amp breaker in the panel or a higher to include derating? If derating is required. What is the percentage?
  5. smoran

    DALI 2 Compliant

    Is the DALI gateway compliant with DALI2? if not will it still work with DALI 2 and what are the limitations?
  6. smoran

    Closed loop daylight harvesting in classrooms on GreenMAX Relay Cabinets

    To cover the basic scenario you explain. Create the area and add the Photocell, Switch, Sensor, and Relays. Assign all the relays to the switch and sensor. (Assuming you want the switch and sensor to control the window relays, if you only want the photocell to control these relays, do not add...
  7. smoran

    I installed the configuration utility for the S7000. But the CT selector box is empty.

    There are TWO configuration utilities, one for the series 7000/7100 and one for the series 7200/7300 The CT pictures and data are stored in a file named "Local" The folder must be located in the local drive root directory. The one for the series 7000/7100 is called "Power Meter Viewer."...
  8. smoran

    GreenMax max # of areas

    Lee, you can have up to 250 areas. Below is a list of all the requirements and max capabilities. MAXIMUM SPEC Notes 1 HDU PER SYSTEM* * A single HDU may host multiple projects) 1 UNIQUE ADDRESS PER SYSTEM 2 TERMINATION JUMPERS per SYSTEM when using...
  9. smoran

    GreenMax max # of areas

    Lee, we need to confirm but there is consensus that it is 64 areas, if you need more I will have to confirm that we can go higher.
  10. smoran

    Network requirements for GreenMAX

    Hello, please see attached for the panel configuration steps. For physical switch requirement: (Ethernet switch?). The panel auto-negotiates, but a managed switch is recommended. Network requirements: Not sure to what requirements you are referring. The panel complies with standard Bacnet and...
  11. smoran

    How to add a user level pin / password

    User-level Pin is assigned on a page basis. this allows the administrator to grant access to pages with different levels of control. If desired the same Pin can be used for every page. From the home page enter the Page Settings Mode. On the bottom center of the screen, press on the Date and...
  12. smoran

    Series 7000 and 7100 master Modbus register list

    Series 7000 and 7100 master Modbus register list
  13. smoran

    GreenMAX Relay Panel - Override for daylight harvesting

    There are no provisions in the programming of the GM panel or Sapphire to override a photocell. the only way to accomplish that is to disable the photocell by cutting the 24+ power supply. You can do this in two ways: 1) No programming is needed, if you add a key switch and run the 24+ wire...
  14. smoran

    Current D4200 Compatibility with old model and remote stations

    Is the current D4200-0LW compatible with a system with a first generation D4200-1LW with a Combine Closure and Remote Stations D42P-RLW?
Back
Top