Hi,
I currently have a PCATR-000 installed in an atrium for daylight harvesting. Do we have a different photocell that has a smaller range? Something that maxes out at 70-foot candles or something in that range?
Hi David,
Is it possible to have two independent timers running? Let's say we want to have channels 1, 2, 3 on a timer and channels 4, 5, 6 on a separate timer. Would this be possible?
This will work on B9 as well correct? The only difference between B9 and B10 is the occupancy sensor will not turn the lights on, it will just detect vacancy.
Questions-
Classroom application with 3 sets of DS relays. The classroom is split into three sections with the lighting: Front, Middle, and Back (Windows). There is a 4-button digital switch in the classroom that gives us ON/OFF plus DIMMING. How would a person set up closed loop daylight...
How hard would it be to have a custom script created so that a Sapphire could have a series of buttons set up for different scenes? Once an individual scene button is pressed, the sapphire will run the scene and then after 6 hours the scene will be turned off automatically. How hard would that...
Just looking for some information regarding the numerator/denominator ratio when creating an open loop daylight harvesting setup. How does the numerator correspond in relation to the denominator? Is there a minimum and maximum range for this? Does it act as a percentage? eg: 50/100 for 50%
Hello,
Working on a larger scale project and seeking some extra information regarding the following for GreenMAX BACnet/BMS integration
Physical switch requirements
Network requirements
Port allocations
Security protocols
External access from BCO group
Let me know if you need any further...
Hello,
Just curious if we have a recommended unit or recommended spec. for a UPS unit to power a GreenMAX Relay Cabinet upon power loss or to power the Cabinet during the transfer switch transition from regular to emergency power.
Working on a GreenMAX application. The idea is we have a large gym with a 4-button digital switch to provide ON, UP, DOWN, and OFF control over the various light fixtures. The customer needs a way of "locking out" control over the 4-button digital switch so that after the lights have been...
This should be fine. The only difference between LC2 and LC3 is software version. When you update the with LC3 software the command module will check the relays and update as needed.
Just wondering how recommended it is to use a DRC room controller to enroll channels from a Relay cabinet and use DRC keypads to control the different relays.
Hi,
Are you able to provide more details on how that would work?
The current setup we have just to give a little more info is the following:
- Photocell is programmed as a trigger point photocell
- CB relays are using B12, ON, Photocell off
- Also have a sapphire connected to the system that...
This site uses cookies to help personalise content, tailor your experience and to keep you logged in if you register.
By continuing to use this site, you are consenting to our use of cookies.