• Does the VRP15 support beaming?

    The VRP03 Z-Wave dimmer supports beaming, such as to security locks. However, I need an appliance module (non-dimming). Does the VRP15-1LW support beaming? If not, are there any plans for it to support beaming in the ...
    created by randman
  • Can the local load controlled by the VRCZ4-MR be CFL?

    I'm interested in getting the Vizia RF + VRCZ4-MR (4-Zone Controller with switch). Can the local load controlled by the switch be a CFL or fluorescent bulb?   Thanks.
    created by randman
  • Using VRI06-1L Dimmer and VP003-10 Coordinating Remote in 3-way

    I have six sets of 3-way lights. I purchased six sets of the matching Leviton Vizia RF + VRI106-1L Dimmer and VP003-10 Coordinating Dimmer (the non-LED version).   The electrician successfully installed the VRI0...
    created by randman
  • Sharing neutral amongst Vizia RF + devices?

    I have a 3 gang box with 3 switches.  One of the  switches in the box has a neutral.  The second switch has no neutral. The third switch, which is part of a 3-way, doesn't have neutral. I'd like to inst...
    created by randman
  • Vizia RF + plug-in modules Questions

    Some questions related to the Vizia RF + plug-in modules:   1. I understand that with the load sensing feature, if the VRP03-1LW plug-in lamp module is currently "off", and you manually turn on the lamp connecte...
    created by randman
  • Vizia RF + dimmers and switches support beaming?

    I see that the new VRC0P that was just released this month supports beaming. Do any of the other Vizia RF + devices support beaming? In particular, the dimmers (e.g. VRI06-1L), switches (e.g. VRS15-1L), and plug-in mo...
    created by randman
  • Vizia RF + dimmer support for dimmable CFL?

    I'm about to replace a large number of switches & dimmers with the Leviton Vizia RF + line. I'm concerned about using the dimmers, however, given that incandescent lights are being "eclipsed" by CFL. So, I'm wond...
    created by randman
  • Okay to use heat tape with Vizia RF+ VRS15-1L switch?

    I live in Northern New York, where heat tape is used in the roof of houses to prevent ice buildup during the cold winter months. The heat tape is currently turned on or off from a switch in the garage. I'm interested ...
    created by randman
  • Vizia RF+ usage on 3-way: neutral needed?

    I'd like to use the Vizia RF+ VRI06 dimmer along with the Vizia + VP00R-10 (no LED) coordinating dimmer remote to replace an existing 3-way dimmer & switch. Is neutral required?   Thanks.
    created by randman
  • VRCPG support for locks (Kwikset, Schlage)

    I've read that a new version of VRC0P is planned which will support locks like Kwikset and Schlage. Are there any plans on having the VRCPG support locks? If so, when, and would it be a firmware update?   Thanks.
    created by randman