• Does Leviton offer a UTP HDMI connector?

    Leviton does offer a HDMI connector in two different wall plate systems. However, neither support UTP terminations as both are feedthrough connectors. The HDMI connector is available in a Decora style insert as well a...
    created by J89
  • What is the diameter size of your splice sleeves?

    The average diameter of each sleeve is:   FSSMI = 0.090” FSSMR = 0.060” Both sleeves are 25 mm in length.   In each tube there is one empty tube to put the fiber in and a metal rod acting as ...
    created by J89
  • Does Leviton offer APC bulkhead adapter plates for ST and FC connectors?

    Leviton does not offer FC adapters.  Leviton does offer ST adapters in our SDX platform.  They are available in 8F or 6F.  The adapters are compatible with Angled Physical Contact connectors as long as ...
    created by J89
  • What size are the cable openings for the Z1000-PF2 zone enclosure?

    The Z1000-PF2 zone enclosure has four cable openings on each of the four sides of the enclosure. The dimension of each opening is 2” X 6.75”.   The spec sheet for this enclosure can be found here: ht...
    created by J89
  • Are Leviton category rated patch cords made of solid or stranded conductor cable?

    Leviton category rated patch cords are made from stranded cable, as patch cords ordinarily require more flexibility.  This is typical throughout the industry. ETL testing showins that the patch cords are componen...
    created by J89
  • What should I do if neither of the windows on the wedge light up?

    First, ensure you have the new “enhanced” Fast-cam connector by checking “SAN” on packaging or check to see if you have the additional 2 & 3mm connector boots that came with the connector k...
    created by J89
  • I have a Telephone Line Distribution Module with a security jack. How is this wired to the security panel?

    From the TLDM security jack, the phone signal is sent over to the security equipment from pins 4&5 and returns back from the security equipment to the TLDM board on pins 1&8.
    created by J89
  • What is the Voltage and amp rating on a 10g patch cord?

    Communications cable is rated for no more than 300v. The Amp rating for a 4 pair 10g patch cable is 1.34.
    created by J89
  • What’s the major difference between the old and new “enhanced” FastCam connectors?

    OLD version      Only can terminate onto 250/900um fiber    Cleave length is 13mm for 900um and 10mm for 250um  Non-VFL compatible     0.2 dB for Insert...
    created by J89
  • Troubleshooting: Internet Gateway /Router / 4-Port Gigabit Router suddenly stopped working

    1. Unplug the power supply from the modem, the Internet Gateway /Router / 4-Port Gigabit Router and shut down your computer. Leave the power off for all devices for approximately 30 seconds.   2. Restart each d...
    created by J89
  • I am unable to log into the Internet Gateway / Router / 4-Port Gigabit Router using the address 192.168.0.1

    1. Check all physical connections between the computer, the Internet Gateway / Router / 4-Port Gigabit Router and the modem   It is helpful to connect the computer directly to the Internet Gateway / 4-Port Gigab...
    created by J89
  • Will the Internet Gateway/ Router / 4-Port Gigabit Router work with a Satellite modem?

    Satellite modems commonly have built-in routers (even when they appear to be 1-port modems). Configuring the Internet Gateway /Router / 4-Port Gigabit Router in a network with a pre-existing router will cause an IP co...
    created by J89
  • Using a wireless router with the Internet Gateway / Router / 4-Port Gigabit Router

    A wireless router can be used with the Internet Gateway / 4-Port gigabit Router. However, some changes will need to be made to the wireless router. If necessary changes are not made to the wireless router there will b...
    created by J89
  • Setting up the Internet Gateway (Version 2)/ 4-Port Gigabit Router for DSL internet

    The following instructions are for 47611-GT4 Version 2 and 47611-GB4. To determine which version you have click here.   For instructions on setup for 47611-GT4 Version 1, call Leviton Tech Support at 1-800-824-...
    created by J89
  • Internet Gateway /Internet Router / 4-Port Gigabit Router Guide

    Logging in to the Internet Gateway (All Versions)/ 4-Port Gigabit Router What version of the Internet Gateway (All Versions) / 4-Port Gigabit Router do I have? How do I upgrade the firmware for the Internet Gateway ...
    created by J89
  • Setting up the Internet Gateway (Version 2) / 4-Port Gigabit Router for Cable Internet

    The following instructions are for 47611-GT4 version 2 and 47611-GB4. To determine which version you have click here.   For Version 3 set-up instructions for cable internet, click here.   For instructions ...
    created by J89
  • How do I upgrade the firmware for the Internet Gateway / Router / 4-Port Gigabit Router?

    To determine what version of the 47611-GT4 device you have, click here   *Note: There is no firmware update released for the Version 3 router at this time. This page will be updated if one is made available. The...
    created by J89
  • Logging in to the Internet Gateway /Router / 4-Port Gigabit Router

    *Important* - Determine which device and version you have before proceeding.   Intial Setup Checklist:   1) Router is powered on 2) The modem is plugged in the WAN port of the Internet Gateway / Router / ...
    created by J89
  • What version of the Internet Gateway / Router / 4-Port Gigabit Router do I have?

    If your device looks like the picture below and is labeled "10/100 Mbps Internet Router", you have the 47611-GT4 version 3       To log into the Internet Router Version 3:   Username field: ...
    created by J89
  • How much weight can the 46700-SLG reclosable J-hook support?

    30 lbs. for every square inch of overlap. Since the Velcro is adjustable, the amount of weight that the J-hook is able to support depends on how much of the Velcro is overlapped. As an example, if there is only 1" inc...
    created by J89