• Need some advice and/or suggestions

    I'm tired of having to walk downstairs to turn off the lights the kids left on (and Lord knows they aren't gonna turn them off!).  I have a three-way switch downstairs that controls about 9 recessed lighting fixt...
    last modified by Robert Lee
  • Motion Sensor

    Bought a ps02 motion sensor switch didn't work on install. I have no ground wires as the house is all greenfield. Any suggestions ?. Would prefer not attaching one.   TY
    last modified by jim sepion
  • Is an IPl06 purchased from Home Depot early 2012 LED Compliant?

    I have wired my entire house with IPl06 dimmers in early 2012.  This weekend I purchased LED bulbs for all of my fixtures.  I was told by an employee that the dimmers must be LED compliant to work properly o...
    last modified by Johnny K
  • Network Protocol Converter (NPC) XP User Guide.pdf

    Please always check for the latest version of this document at https://www.leviton.com/ (use the site search)
    last modified by Alan Moss
  • Network Protocol Converter (NPC) DLR User Guide.pdf

    Please always check for the latest version of this document at https://www.leviton.com/ (use the site search)
    last modified by Alan Moss
  • Provolt™ Ultrasonic Line Voltage Occupancy Sensors Product Specifications

    Please always check for the latest version of this document at https://www.leviton.com/ (use the site search) Learn more about Provolt Occupancy Sensors at https://www.leviton.com/provolt
    last modified by Alan Moss
  • Provolt™ PIR Line Voltage Occupancy Sensors Product Specifications

    Please always check for the latest version of this document at https://www.leviton.com/ (use the site search) Learn more about Provolt Occupancy Sensors at https://www.leviton.com/provolt
    last modified by Alan Moss
  • Provolt™ Multi-Tech Line Voltage Occupancy Sensors Product Specifications

    Please always check for the latest version of this document at https://www.leviton.com/ (use the site search) Learn more about Provolt Occupancy Sensors at https://www.leviton.com/provolt
    last modified by Alan Moss
  • How do I make a shorting plug for the security jack on the telephone line distribution board?

    How do I make a shorting plug for the security jack on the telephone line distribution board?  
    last modified by gabby
  • Can I place additional GFCIs on multiple bathrooms on same 15A circuit that has one GFCI?

    My house was built around 1990. There are three bathrooms that have 4 outlets all at sinks and 2 outside outlets. All the outlets are on one 15A circuit. one of the baths upstream has the one GFCI protecting everythin...
    last modified by Barry Cavin
  • Wiring a 3 way IPV15 switch

    I'm installing an IPV15 and IPVOR in a hallway. Theres only one wire in the IPV15 box. Coming from the IPVOR switch  there's the Black hot wire, White Neutral, Red which is coming from the 3 way connection and a ...
    last modified by Benny Beronda
  • GFCI breaker install

    Just replaced a 20 amp GFCI outlet from LEVITON.  Test and reset buttons will not set. Also reading voltage with my light stick on both sides of the outlet.  Is this a bad outlet or possible bad circuit brea...
    last modified by randy hedrick
  • What do I need

    I need to replace a bad plug on a compact dryer.   It connects to a standard 110v outlet.     The plate on the dryer states the connection is "120v 12A 60hz 3-wire connection" This is writ...
    last modified by sandy jackson
  • Dimmer doesn't shut off the lights completely

    I've install a MDM06-1LW dimmer with a Zurik 24V  Magnitude’s Magnetic LED Driver to operate a run of Flexfire LEDs 71 watts and 3 amps. The switch works fine to turn up or down the lights. However when I...
    last modified by Kenny Lind
  • 5634 Leviton decora -two switch unit

    I am installing this new switch to replace one that broke (toggle)..  Does the red wire connect to the top or bottom black screw on the left hand side of the switch?  The other wire is black.
    last modified by Michael Ecker
  • Why does it pop on first activation?

    I have purchased 2 Leviton dimmers recently. Both went into LED lighting, one with 7 75W equivalent and the other with 2 60W equivalent lights. Both times when I first turned on the lights there was a pop. It was a mo...
    last modified by Geoffrey Kloster
  • Looking for a solution to use an occupancy sensor for stairwell lighting

    Hello,   I'm looking for a solution to a light switch problem I am having with the stairwell that goes from the main floor to the upper floor in my home.  Currently, I have an occupancy sensor (I believe it...
    last modified by Shin
  • GFCI to downrate a circuit

    I have a 20A circuit that ends at a duplex that I would like to then feed a 15A circuit.  Can I use a 15A GFCI to essentially convert that 20A circuit to a 15A circuit at that duplex?
    last modified by Mel Hoke
  • Wiring a GFCI when there are 2 hot lines and a neutral coming into current receptacle

    I need to install GFCI plugins on either side of my kitchen sink (older home). The problem  I have run into is that each of the current receptacles is wired with two hot lines in such that the upper receptacle is...
    last modified by Jim Kelly
  • Vizia RF+ Installer Tool and compatibility with Monster Illuminessence dimmers, RCS TZ43 thermostat and Intermatic CA9000 motion sensors.

    I have recently taken delivery of a VRUSB-1US Installer Stick, and downloaded version 1.0.4 of the Vizia RF+ installer software, which I used it to set up my partially completed ZWave network.  The network curren...
    last modified by Odeen