Log in to follow, share, and participate in this community. Not a member? Join Now!
Thread Omni Pro Motions
Omni Pro MotionsI am working with an Omni Pro and the two motions keep saying not ready? I've added the 1k ohm resister. Any suggestions on what to do?
HomeseerI read the article "Using Amazon Alexa to Control an Omni Automation Controller" via Homeseer. My question is whether at that point OmniPro II acts still as a controller or the controller now is Homeseer. What happens...
Vision Z-Wave Relay issue (ZL7432US)System Motion Detector triggers Z-Wave relay that turns on Flood Lights and sends status to OmniPro II. (replacing old X-10 PR511 Flood Light functionality) I have 3 Vision Z-Wave relays (Single Version ZL743...
Thread Omni Pro II Humidity Control for Wine Cellar
Omni Pro II Humidity Control for Wine CellarI seek advice on how to set a Omni Pro II rev 3.8 humidity zone for 45%RH not ready and 55% ready state? This is to control a wine cellar humidifier via X-10 unit.
Cellular support in Omni IIeI'd like to move away from my landline monitoring which costs around $45/mo plus the monitoring fees from the central station which I'm hoping will be cheaper per month. What products would work with the Omni ...
Omni-Link II protocol documentsHas Leviton/HAI published any up to date Omni-Link II protocol description documents? The only version of this document that I can find is dated October 2009. Thanx
OmniPro II & CrestonIs anyone running the creston product with their omnipro II? Looking for some feedback on the creston product with its integration with the OmniPro.
IR controlI need to have some basic IR control from an Omnipro 2 serial port, turn on/off stereo when arming, etc. Any suggestions of third party devices?
Omni Pro IIWe have using Omni Pro II Controller with 4 stes of 16IN/OUT Expansion Board. Please advise in the following questions. 1. When the communication cable between Omni Pro II and 16IN/OUT Expansion Board is disco...
Help Spec my Omni Security SystemI've narrowed down my search for a security system, but need help confirming my setup to make sure everything is compatible and I have enough room to grow as the system expands. Sensors: - (3) Zwave door sens...