• Homeseer

    I read the article "Using Amazon Alexa to Control an Omni Automation Controller" via Homeseer. My question is whether at that point OmniPro II acts still as a controller or the controller now is Homeseer. What happens...
    Florin Musat
    created by Florin Musat
  • Vision Z-Wave Relay issue (ZL7432US)

    System Motion Detector triggers Z-Wave relay that turns on Flood Lights and sends status to OmniPro II. (replacing old X-10 PR511 Flood Light functionality)   I have 3 Vision Z-Wave relays (Single Version ZL743...
    James Allison
    last modified by James Allison
  • Configuring the Leviton Omni Notifier Using My Leviton Cloud

    In order to configure a Leviton Omni Notifier using the My Leviton cloud, you must have the following:     1. My Leviton Account     2. Leviton automation controller running firmware version 3.16...
    Scott Dudoussat
    last modified by Scott Dudoussat
  • Using Amazon Alexa to Control an Omni Automation Controller

    Description:   This integration note will describe how to control Lighting (Control), temperature (Thermostats), and macros (Buttons) on an Omni controller with voice commands using an Amazon Echo or Dot and a H...
    Scott Dudoussat
    last modified by Scott Dudoussat
  • PC Access will not Run on new Windows 10

    Just upgraded from W7 ro W10.  PC Access will now not work.  Windows just says "... has stopped working". Any ideas
    last modified by Andrew bush
  • Omni Pro II Humidity Control for Wine Cellar

    I seek advice on how to set a Omni Pro II rev 3.8 humidity zone for 45%RH not ready and 55% ready state?  This is to control a wine cellar humidifier via X-10 unit.
    last modified by Jon Gonzales
  • how to downgrade the PC Access

    hello, does anybody know to downgrade the pc access to lower version?
    last modified by robert sanantonio
  • Cellular support in Omni IIe

    I'd like to move away from my landline monitoring which costs around $45/mo plus the monitoring fees from the central station which I'm hoping will be cheaper per month.   What products would work with the Omni ...
    last modified by Michael Skvarenina
  • Omni-Link II protocol documents

    Has Leviton/HAI published any up to date Omni-Link II protocol description documents?  The only version of this document that I can find is dated October 2009.   Thanx
    last modified by Bob Sutnavage
  • OmniPro II & Creston

    Is anyone running the creston product with their omnipro II?  Looking for some feedback on the creston product with its integration with the OmniPro.
    last modified by Steve Walsh
  • Leviton Pro-Link Description

      DESCRIPTION   Pro-Link is a programmable protocol whose messages can be programmed into a Leviton automation controller. Using Pro-Link, a Leviton automation controller can send commands to and interpret c...
    Ernie Sieber
    last modified by Ernie Sieber
  • Does PC Access 3 come in different languages?

    Question:   Is PC Access available in different languages?   Answer:   Yes.  PC Access 3 has built in support for several languages and does not require a special version for supported languages...
    Ernie Sieber
    last modified by Ernie Sieber
  • KPL-7 Scene Switch Installation Tips

    The following tips can be time saving in the proper setup and operation of the RCS KPL-7 Seven Button Scene Switch. This article is for controllers with 2.15a or older firmware. KPL7 support is built into controllers ...
    Ernie Sieber
    last modified by Ernie Sieber
  • Integrating a RadioRA 2 Lighting System to a Leviton Controller, Controller Firmware 3.4

    INTRODUCTION   Leviton Omni and Lumina family controllers support two-way integration with the Lutron RadioRA 2 lighting system. Individual lights can be directly controlled and lighting scenes can be triggered ...
    Scott Dudoussat
    last modified by Scott Dudoussat
  • Why does my PC Access software modem connection end when I hang up the phone?

    Question:   Why does my PC Access software modem connection end when I hang up the phone?   Answer:   You probably have a phone improperly connected to the PC modem.  Most PC modems have...
    Ernie Sieber
    last modified by Ernie Sieber
  • Error Occurred On Init. Command 1

    Symptoms   When attempting to use PC Access through a modem connection, "Error occurred on initialization command 1" is displayed.   Cause   This error is directly related to the inability of ...
    Ernie Sieber
    last modified by Ernie Sieber
  • Modems Will Not Handshake When Accessing Controller Via PC Access

    Problem:    When accessing a Leviton controller via modem, the controller and computer modems will not handshake.   Troubleshooting Steps:    In PC Access, click on Configure/Modem ...
    Ernie Sieber
    last modified by Ernie Sieber
  • Common Modem AT Command Strings

    Error Correction Commands   Error correction helps cut down on noise and other phone line problems, which will result in less data loss. The packet design of error correction can also lead to greater throughpu...
    Ernie Sieber
    last modified by Ernie Sieber
  • PC Access 3.0 Crashes After First Use

    Problem Summary:   After installation, PC Access version 3.0 is opened and used without issue.  After using the software and closing the program, it can no longer be opened without receiving an error lik...
    Ernie Sieber
    last modified by Ernie Sieber
  • Sleep Mode Restored/Disabled

    Question:   What do the "System Sleep Mode Enabled" and "System Sleep Mode Disabled" messages displayed in the lower-left corner of the PC Access screen mean?   Answer:   These messages are r...
    Ernie Sieber
    last modified by Ernie Sieber