Skip navigation

Tags:

pr180
Sort by: Frequency Name What:

Content tagged with pr180

Subject Author
Re: PR180 Buzzing 2 months ago in Occupancy Sensors by Rob Ramirez Rob Ramirez
Re: pr 180 wiring diagram (line side) 9 months ago in Occupancy Sensors by Ryan Lundbom Ryan Lundbom
Re: PR180 3-Way Wired Wrong 3 months ago in Occupancy Sensors by `Hugh Vail `Hugh Vail
Re: PR180 installation problem 1 year ago in Occupancy Sensors by Leviton Technical Representative Leviton Technical Representative
Re: Help with a PR180 3-way issue 2 years ago in Occupancy Sensors by Leviton Technical Representative Leviton Technical Representative
Re: PR-180 Installation Problem/Question 1 year ago in Occupancy Sensors by Tom Burton
Re: Can the pr 180 be installed in either switch position in a 3-way? 1 year ago in Occupancy Sensors by dcandmc
Re: PR 180 photocell problems 2 years ago in Occupancy Sensors by bcarberry bcarberry
Can the PR150 and PR180 wall switch sensors be used with compact fluorescent lamps? 2 years ago in Occupancy Sensors by PCP
Re: Can I wire two PR180's together? 2 years ago in Occupancy Sensors by Kertdigg Kertdigg
Re: In a 3-way application, if the PR180 is in the off position will the standard 3-way switch be able to turn the lights on? 3 years ago in Occupancy Sensors by Leviton Technical Representative Leviton Technical Representative
Re: Can the residential wall switch sensors (PR180 & PR150) be used to control compact fluorescent bulbs or electronic ballasted fluorescents? 3 years ago in Occupancy Sensors by Leviton Technical Representative Leviton Technical Representative
Re: Why is my fluorescent lighting flickering when the PR180 is in the auto position but when set to the on position the flickering stops and lighting remains fully lit? 1 year ago in Occupancy Sensors by Bart D
Re: Are the PR180 and PR150 both capable of switching motor loads or exhaust fans? 3 years ago in Occupancy Sensors by Leviton Technical Representative Leviton Technical Representative
Re: Is there a minimum load requirement for the PR180 & PR150? 3 years ago in Occupancy Sensors by Leviton Technical Representative Leviton Technical Representative
Re: Can a PR180 be used in a 3 way with another PR180? 3 years ago in Occupancy Sensors by Kertdigg Kertdigg