• What is the difference between a 5-20P and a L5-20P?

    A 5-20P is a standard straight prong plug or receptacle. If there is a L in the plug or receptacle description such as L5-20P  this tells you that it is a Locking style outlet. Locking means the once the plug is ...
    last modified by zacsmith
  • What is a locking plug?

    A locking plug is a plug that inserts into a receptacle and then twists in order to lock it into place, this prevents any accidental disconnection. To remove the plug simply twist in the oposite direction and remove f...
    last modified by zacsmith
  • When will FLX PDUs be available?

    Production of the FLX series PDU line has been put on hold till further notice. They have not been Discontinued , they will be available at a future date to be announced. Contact technical support for more information...
    last modified by zacsmith
  • FLX Firmware updates

    There are no FLX series PDU firmware updates at this time.
    last modified by zacsmith
  • How many Brackets do I need to order to mount a vertical PDU?

    A vertical PDU requires 2 brackets to be mounted. Each bracket kit PDURK-BKT includes 2 brakets so you only need one (1) kit for each vertical PDU.
    last modified by zacsmith
  • Do the metered PDUs tell individual outlet use?

    No, the metered PDUs do not meter individual outlet use. They only meter the combined aggregate use of power used on all outlets on the PDU.
    last modified by zacsmith
  • I need a PDU with a thermal fuse

    If you need a PDU with thermal fusing you can choose from either the SWITCHED series Levtions PDUs or the METERED series Leviton PDUs. Any PDU from the SWITCHED or METERED series will have thermal fusing. Please conta...
    last modified by zacsmith
  • Switched PDU

    Do the Switched series PDU's have current monitoring for each individual outlet?
    last modified by RS9
  • Is the fuse on a Leviton switched horizontal PDU replaceable?

    The fuse on our switched series PDU's is not designed to be user-replaceable.  Please contact Technical Support for more information at 800-824-3005.
    Darby
    last modified by Darby
  • Horizontal PDU in a 23 inch rack

    Do Leviton Horizontal PDU's come in different sizes so that they fit in a 23 or a 19 inch rack? is there a adapter bracket?
    last modified by DESTRO
  • PDU enviromental sensors

    Some of the Leviton PDUs have the capability of using enviromental sensors, what is the part number and how do they connect to the PDU?
    last modified by DESTRO
  • How do I replace a fuse in a switched series PDU?

    I have a switched series PDU with a blown fuse, how do I replace it?
    last modified by DESTRO
  • PDU MIB

    I need the MIB for seting up my Leviton PDU, is it available?
    last modified by DESTRO
  • What is a Modular power cord?

    I saw in the leviton catalog that some of the PDUs require a modular power cord, what does this mean?
    last modified by DESTRO
  • what is a " Switched " PDU?

    I noticed in the leviton catalog there are several options for PDUs, what does it mean when it says Switched?
    last modified by DESTRO
  • what is a " Basic " PDU?

    I noticed in the leviton catalog there are several options for PDUs, what does it mean when it says Basic?
    last modified by DESTRO
  • What is a monitored PDU?

    I noticed in the leviton catalog there are several options for PDUs, what does it mean when it says monitored?
    last modified by DESTRO
  • what is a " Metered " PDU?

    I noticed in the leviton catalog there are several options for PDUs, what does it mean when it says  metered?
    last modified by DESTRO
  • What do I need to know when choosing a PDU?

    Before choosing a power distribution unit, it's helpful to understand the application and have answers for the following questions:   Do you need an enhanced metered, metered or basic PDU? Will the PDU be moun...
    last modified by J89