• MDP and SJP fiber cable options for fiber trunks?

    What's the difference between these options, and when would you select each?
    Darby
    last modified by Darby
  • Splicing in 5WMNT-1C?

    Does the 5WMNT-1C accept splice trays?
    Darby
    last modified by Darby
  • Fiber Enclosure for DIN rail?

    Does Leviton offer a product to mount fiber on a DIN rail?
    Darby
    last modified by Darby
  • How is GPON distributed?

    What is a typical GPON scenario look like?
    Darby
    last modified by Darby
  • Interoperability of MPO and MTP cables?

    Is there any interoperability issue between different manufacturers of MPO/MTP pre term cables. Think harness to trunk interface at a feed thru. Specifically as it relates to the degree of angle polish on the face of ...
    Darby
    last modified by Darby
  • Does Leviton offer an APC (Angled Physical Contact) pre-polished connector?

    If so, what is required for termination?
    Darby
    last modified by Darby
  • MTP Singlemode - UPC or APC?

    Are the MTP singlemode connectors used by Leviton UPC (Ultra Physical Contact), or APC (Angled Physical Contact)?
    Darby
    last modified by Darby
  • Bare Fusion Splice Chips (Holders)

    I am using Leviton bare fusion splice chips with 250µm buffered fiber.  After inserting the spliced fibers into the chip I am having an issue with both retention and breakage.  The fibers will not stay...
    last modified by Mat Gallien
  • Front cable management for e2xhd panel?

    Is there a cable management tray that will mount to the front of a flat e2xhd panel, such as the E2X1F-D48?
    Darby
    last modified by Darby
  • Difference between Replicator 1U and Standard 1U FM Panel

    What is the difference between the two part numbers:   RPL-BRCD48PLCM4 Replicator, Brocade 48 Port Blade, 8 x MTP-LC, OM4, 1U, Black, MTD A and FM-F096CAB0A   Fiber Plug-n-Play MTP Module, 96-f...
    Darby
    last modified by Darby
  • What is the ST Fastcure Connector made from

    What type of metal is used on the barrel?
    Darby
    last modified by Darby
  • Patch-cord Serial Number Recording?

    I notice that all of the fiber patch-cords used in our installation have a serial number.  Do I need to document/record all of the serial numbers to comply with ANSI/TIA standards?
    last modified by Mat Gallien
  • Why does the Leviton SC/APC FastCAM Connector Require a Special Cleaver?

    The instruction sheet for the Leviton SC/APC cleaver states than a special "Angled" cleaver must be used during termination.  Why is this?
    last modified by Mat Gallien
  • Mating Cycle Testing on FastCam 49991?

    How many mating cycles are Leviton FastCam connectors tested to?
    Darby
    last modified by Darby
  • Mating Cycle Testing - FastCure 49990 connectors

    How many mating cycles are Leviton FastCure connectors tested to?
    Darby
    last modified by Darby
  • 24 fiber Splice cassettes and Opt-X Core cassette A/B polarity description

    When looking at the cassette with Ports 7-12 on the top, the top row of the Splice cassette is "Key Up"  while the bottom row is "Key Down". This is done so the user has access to the release tabs on the LC conne...
    Darby
    last modified by Darby
  • HDX to e2XHD cassettes and polarity

    When you have a HDX cassette (adapter is key up) on one end and an e2XHD cassette (adapter is key down) on the other end, shooting a VFL down fiber one (the left port of the #1 adapter) on the HDF will result in it sh...
    Darby
    last modified by Darby
  • Fastcam connectors with loose tube fiber - tips!

    Terminating Fastcam connectors on loose tube fiber will require the 250um fibers to be built up to 900um using a fanout kit, such as 49887-12S. You will want to leave2-4mm of 250um coating extending beyond the 900...
    Darby
    last modified by Darby
  • Calculating Savings on HDF3168 vs Standard Infrastructure

    Why use the HDF3168 versus more traditional patch and splice solutions? Is the cost savings really significant?
    Darby
    last modified by Darby
  • Difference between OM4 and OM4+?

    What is the difference between these fiber types? How can you tell them apart?
    Darby
    last modified by Darby