• Patch cord length for Auto switching wallplate

    Customer would prefer to connect direct to auto switching wall plate with horizontal cable instead of using small patch cord unless patch cord is 6 inches long.  Does Leviton make that short of a patch cord that ...
    last modified by Darby
  • Do Leviton HDMI Extenders support 4K, 8K and 16K?

    Specifically the 41910-HTE and 41910-HT0?
    last modified by Darby
  • 11.     USB port on auto switching wall plate?

    Is the USB port on auto switching wall plate 41920-HRC only for keyboard & mouse use?  Not for i-Pods or any other device?
    last modified by Darby
  • HDMI CEC Control and Leviton extenders?

    HDMI extenders and  CEC control?
    last modified by Darby
  • Does DVI-D carry audio?

    Does DVI-D carry audio?
    last modified by Darby
  • Maximum Amps HDMI extender will see over the PoH (worst case scenario)?

    What is typically the maximum Amps your HDMI extender will see over the PoH in worst case scenario (from a safety perspective if kids get into the conductors on the UTP cable)?
    last modified by Darby
  • HDMI over Category rated cable?

    Does Leviton offer anything to handle HDMI over Category cable?
    last modified by Darby
  • E2XHD-CMB cable manager mounting

    How does the E2XHD-CMB cable manager mount?
    last modified by Darby
  • 4K HDMI Feed-thru

    Do you offer an HDMI feed-thru insert that can pass 4K signal?
    last modified by Darby
  • Voltage rating on patch cords?

    What is the voltage rating on your copper patch cord jackets?
    last modified by Darby
  • 41297-2P* opening?

    What size is the hole on the 41297-2PW pass-thru MOS module?
    last modified by Darby
  • What diameter of cable will Atlas X-1 jacks accept?

    What diameter of cable will Atlas X-1 jacks accept?
    last modified by Darby
  • FT4 vs FT6... what to use when and why?

    FT4 vs FT6... what to use when and why?
    last modified by Darby
  • Does Leviton offer a "Smart" patch system

    For example, a patching system that connects to a local network for monitoring ports?
    last modified by Darby
  • Shielded jack shorting?

    Why am I getting a short when testing my shielded jack?   6S180-SH6 6S10G-S6A 5S180-SH5
    last modified by Darby
  • High Flex 6 patch cords and poe+

    Can the high flex patch cords (HD6 6H460) which are 28-gauge cable, be used for both POE and POE+
    last modified by Darby
  • ians9701

    Can I use a Leviton 5G108-RL5 Cat5e Snap in jack with stranded Cat5 cable?
    last modified by Ian Swirsky
  • What is the vertical flame test for CMR Cables?

    UL-1666 is the Vertical Flame test for Riser cables, so any cable rated CMR (Riser-rated) could be deemed to have passed this UL test. IEC 60 332-3 and EN 50226 are the European counterparts to the UL-1666. Both are v...
    last modified by DU0
  • What is the Voltage and amp rating on a 10g patch cord?

    Communications cable is rated for no more than 300v. The Amp rating for a 4 pair 10g patch cable is 1.34.
    last modified by J89
  • Voice Patch Panel 1RU, 49013-xxx

    Dear all,   Please if anyone have more informations and details about Voice Patch Panel 1RU, 49013-xxx send to me, also I need to know if I can use it for Cat3 termination or no ???     thanks a lot
    last modified by Ayman Ramadan