• How long are the velcro straps in 41010-SPW?

    The saddle ties include a 8 inch long by .5 inch wide velcro strap.
    last modified by zacsmith
  • How long is the velcro strap in the saddle ties 41020-SPR ?

    The Saddle ties have a 8 inch long by .5 inch wide velcro straps included with purchase.
    last modified by zacsmith
  • Can the part number 49005-CMB bolt on to the rack?

    No this cannot mount to the rack only to the patch panel.
    last modified by TML
  • Can the Fiber race way system be used for copper networks?

    Yes the fiber race way system can be used with copper but there are a few things to keep in mind. Copper cables are much heavier than the fiber optic cables the system is typically used with. Generally 1 circuit (1 ca...
    last modified by zacsmith
  • How much weight can the 46700-SLG reclosable J-hook support?

    30 lbs. for every square inch of overlap. Since the Velcro is adjustable, the amount of weight that the J-hook is able to support depends on how much of the Velcro is overlapped. As an example, if there is only 1" inc...
    last modified by J89
  • Is there a front cable managment bar for your angled patch panels?

    There is no cable manager designed to go on the front levitons angled patch panels. This is because the idea behind a angled patch panel is to allow a more direct path to the cable manager and to ease stress on the ca...
    last modified by zacsmith
  • How can I figure out cable density for my cable manager?

    There is a cable density chart available on page A89 of the 2011 Network infrastructure solutions. Please see link below http://www.leviton.com/OA_HTML/ibeCCtpSctDspRte.jsp?section=28178&minisite=10028
    last modified by zacsmith
  • Can I purchase Versi-Duct replacment covers?

    The standard black covers that come with the 5 inch  horizontal and vertical Versi-Duct system is not available seperatly. The only cover we have seperatly is the optional grey designer covers 59265-5DC for the 5...
    last modified by zacsmith
  • What standards address cable support in a drop ceiling?

    The applicable Standard is TIA-569-B (2004) Commercial Building Standard for Telecommunications Pathways and Spaces Section 8.7. This Standard recommends supports at intervals that are not to exceed 5 feet. Additional...
    last modified by J89
  • How much distance should be between electrical wiring and low voltage wiring?

    The TIA standards have gone away from calling out actual distances to deferring to the National Electrical Code.  The only distance limitation that can be found in the National Electrical Code calls out a 2&rdquo...
    last modified by J89
  • Can I run power and data in the same conduit?

    The NEC Article 725.55(A) does not allow running Class 2 and Class 3 circuits with power, lighting or Class 1 circuits in the same cable or raceway, except for very limited cases.  One circumstance where it is al...
    last modified by J89
  • How do I mount verticle cable managers between two racks?

    Certian applications call for verticle cable managment between two free standing racks. But the 4980L, 4940L and 8980L series managers ship with brackets attached to one side of the cable management only.   The ...
    last modified by J89