• Speaker DC Resistance

    I recently purchased a Leviton Mixing Audio Amplifier and two sets of 8-Ohm speakers.  Before connecting the amp and the speakers I wanted to make sure the speakers were configured correctly.  I used a DIMM ...
    last modified by Mat Gallien
  • HDBaseT Extenders and IR Kits

    I've purchased the Leviton 70m transmitter & extender kit (41910-HT0) and I would like to pass IR control signals from one side of the link to the other.  I found an IR kit online--it is not Leviton's--will i...
    last modified by Mat Gallien
  • Wallplate for multiple cable pass-through

    Does Leviton have an option for passing multiple cables through a wallplate?  For example, if I want to pass HDMI & component video cables to the rear of my TV?
    last modified by Mat Gallien
  • British Style Shuttered Inserts, LI150

    Are all Leviton AV adapters compatible with Leviton British Style Shuttered Inserts?
    last modified by Mat Gallien
  • 41920-HRC, Directly Connected to Display

    I would like to use the Leviton Auto-Switching Wallplate without the suggested HDBaseT receiver.  The projector we are using has an HDBaseT port.  Can I connect the output from the Auto-Switching Wallplate d...
    last modified by Mat Gallien
  • HDBase-T Extender Distances

    What are the maximum distances the Leviton HDBase-T devices support?
    last modified by Mat Gallien
  • MTO Products?

    I received a Leviton quote and I notice some of the items are called MTO?  What are MTO items?
    last modified by Mat Gallien