Click here for quick access to several helpful topics on the Leviton 47611-GT4 4-port Internet Router or Internet Gateway, and 47611-GB4 Gigabit Router.
You will find installation and setup instructions, as well as tips and suggestions for troubleshooting.
Expiring the announcement will not delete it but will remove it from the public announcement list. Are you sure you want to expire this announcement?
Are you sure you want to delete this announcement?
Log in to follow, share, and participate in this community. Not a member? Join Now!
Thread What is subnet?
What is subnet?Subnet is a portion of a network that shares a common address component. On TCP/IP networks, subnets are defined as all devices whose IP addresses have the same prefix. For example, all devices with IP addresses that ...
Thread What are the advantages and disadvantages of DHCP?
What are the advantages and disadvantages of DHCP?DHCP is Dynamic Host Configuration Protocol which use to assign the IP address Dynamically and Automatically in system Advantages All the IP configuration information gets automatically configured for your&n...
What is DNS?Short for Domain Name System (or Service or Server), an Internet service that translates domain names into IP addresses. Because domain names are alphabetic, they're easier to remember. The Internet however, is really...
What is DHCP?Short for Dynamic Host Configuration Protocol, a protocol for assigning dynamic IP addresses to devices on a network. With dynamic addressing, a device can have a different IP address every time it connects to the net...
What is a MAC address?The address for a device as it is identified at the Media Access Control (MAC) layer in a computers internal network architecture . MAC address is usually stored in ROM on the network adapter card and is unique to eac...
Thread Whats the difference between Static and Dynamic IP settings?
Whats the difference between Static and Dynamic IP settings?Dyanmic Routing is used to have the best path no matter what the status of the physical links. All routers have some sort of shortest-path or lowest-cost or best-choice algorithm to weigh all the options available. St...
What is a modem?A device that converts digital signals for transmission over analog carrier lines. Modems provide computer access to the Internet through cable or basic phone lines.
What is Integral BridgingA technique that combines different media and topologies. It requires the installation of additional network interface cards in a server.
Thread What is the pull force when installing wire?
What is the pull force when installing wire?Do not use more than 25 lbs of pull force when installing this wire it can cause the twists in the pairs to unravel reducing reliability and speed
What is Cat 6a?Cat 6a has even more shielding and the diameter is greatly increased due to this. This wire has a lot lower flexibility than Cat 6 or any other UTP wire due to this. Cat 6a is rated at 10 Gbps past 100 fee...
What is Cat 6?Cat 6 wire is a 23 gauge four pair wire. Cat 6 is rated at speeds of up to 10 Gbps at 100 feet after 100 feet this drops to 1000 Mbps or 1 Gbps. Cat 6 generally has a plastic core keeping the proper twists...
What is Cat 5e?Cat 5e is very similar to Cat 5 it contains more twists per inch and is capable of transmitting data at a rate of up to 1000 Mbps or 1 Gbps. We recommend running two Cat 5e wires to each wall outlet in their hom...
What is Cat 5?Cat 5 is a 24 gauge four pair wire that can support either 4 line phone service or data. Cat 5 is rated at speeds of 100 Mbps and is backwards compatible with Cat 3 or POTS.