Click here for quick access to several helpful topics on the Leviton 47611-GT4 4-port Internet Router or Internet Gateway, and 47611-GB4 Gigabit Router.
You will find installation and setup instructions, as well as tips and suggestions for troubleshooting.
Expiring the announcement will not delete it but will remove it from the public announcement list. Are you sure you want to expire this announcement?
Are you sure you want to delete this announcement?
Log in to follow, share, and participate in this community. Not a member? Join Now!
Leviton Router & Switch and PoEI'm adding a PoE switch to my setup to connect a number of IP Cameras. I'd like to connect the PoE switch to the Leviton switch I already own. Can the PoE switch damage the (non-PoE) Leviton switch?
Wireless Router, 47611-WG4 Password LimitsI have the 47611-WG4 Leviton Wireless Router. I recently set my admin password to a 24 character password. After logging out, I was unable to log back in. I had to factory reset the modem using the W...
Thread Why is my picture dim when using the MOS VGA modules?
Why is my picture dim when using the MOS VGA modules?This is caused by the impedance balancing internals of the connectors. Adjust contrast higher on equipment. Adjusting contrast is a by product and has no ill effects.
Wiring Voice and Data QuestionsI'm in the process of trying to figure out how to install a structured cable system. Mainly it is to make it neater (currently just a bundle of wires hanging from the ceiling), but also to be able to switch part...
What connects to what?I am getting ready to build a home and wire the CAT5e and RG6 Quad myself. I have purchased a 42" Leviton SMC, a Leviton 476TM-524 Patch Panel, a Leviton 47611-GT4 Router, a Leviton 47605-DP AC Power Module, a Leviton...
47611-GT4 Router (Version 3) DNS SettingsWe recently installed the 47611-GT4 (v2) router to terminate a cable modem. We opted to use the default settings and make no configuration changes. Our clients received IP addresses within the 192.168.0.x space, howev...
Thread Setting up the 4-Port Internet Router (Version 3) for Cable Internet
Setting up the 4-Port Internet Router (Version 3) for Cable InternetThese instructions pertain ONLY to Version 3 of the 47611-GT4 Internet Router. To determine which version you have, click here. 1) Log in to the router. Instructions for logging in can be found here. Once log...