Large MOS Surface Mount BoxCan I use large AV connectors such as the MOS VGA connectors 41295-VM*, 41295-VP*, or 41295-HD* with the large MOS (3-MOS) Surface Mount Box?
Structured Media Enclosure Power ModulesI notice that the two types of Structured Media Enclosures, metal (47605 series) & plastic (49605 series), have different knockouts in the bottom. Which power modules can I use with each of these enclosure t...
Knockouts on MDU EnclosuresWhat are the knockout sizes on the Configuration A and Configuration B MDU style Structured Media Enclosures? PN 47605-4MG 47605-M42 47605-2MG 47605-M28
Thread Universal shelf bracket does not fit in media enclosure
Universal shelf bracket does not fit in media enclosureI just received a structured media enclosure (47605-28N), and a universal shelf bracket (47612-UBK) that I ordered through Amazon. However, the holes on the bracket do not line up with the holes in the enclosure...
Need helpI purchased an 11-year old home that has a Leviton structured media system with built in speakers installed in several rooms. Alas, no instructions or audio equipment were included with the house. ...
Thread Do 110 to RJ45 patch cords fit on Leviton's residential 110 boards?
Do 110 to RJ45 patch cords fit on Leviton's residential 110 boards?Yes they do fit, however, using these to test the boards can sometimes damage the circuits. It requires much more force to pull them off then to put them on. The process of removing the 110 cable can cause the circuit...
Thread How do I set the 47611-GTY back to factory default settings?
How do I set the 47611-GTY back to factory default settings?Step 1. Unplug the power cable from the router. Step 2. Plug one end of an ethernet/patch cable into port 1 and the other end of the same cable into port 4. Step 3. Press and release the uplink button....
Cat 5e Voice and Data Board NumberingThe Leviton Category 5e Voice and Data board is a common piece in many of our Structured Media Center preconfigured panels. As shown below, the terminations correspond to ports 2,4,6 on the left, and 1,3,5 on th...
What sizes do your SMC come in?I have a 14" structured media center that was in my house when I moved in. I want to expand my system so Iam going to need more room in my enclosure.Do you offer any other sizes?
Component placementWhere do you install the Westell modem in the structured wiring panel box? This is my very first installation ever. I know residential power distribution; this is new horizons for me! I'll be installing an Internet, ...