• Concrete Structured Media Enclosure Knockouts?

    What are the size of the knockouts on the concrete-mountable SME? Where do you install a power outlet?
    Darby
    last modified by Darby
  • Large MOS Surface Mount Box

    Can I use large AV connectors such as the MOS VGA connectors 41295-VM*, 41295-VP*, or 41295-HD* with the large MOS (3-MOS) Surface Mount Box?
    last modified by Mat Gallien
  • 40540 Cat 5e wiring?

    How do I read the wiring label on the 40540 wallplate for the Cat 5e jack?
    Darby
    last modified by Darby
  • Cable Management in Structured Media Enclosure?

    What is the recommended method for cable management inside the Leviton Structured Media Enclosure?
    Darby
    last modified by Darby
  • Cable Management in Structured Media Enclosure?

    What does Leviton recommend for cable management inside an SMC?
    Darby
    last modified by Darby
  • What is the operating temperature for the 47613-EZ6?

    What is the operating temperature of the Cat 6 EZ RJ45 plug?
    Darby
    last modified by Darby
  • What are the knockouts on the concrete enclosures?

    What type of knockouts are on the concrete-mountable structured media enclosures? For example pn 48605-21E, 48605-28E, 48605-42E
    Darby
    last modified by Darby
  • Structured Media Enclosure Power Modules

    I notice that the two types of Structured Media Enclosures, metal (47605 series) & plastic (49605 series), have different knockouts in the bottom.  Which power modules can I use with each of these enclosure t...
    last modified by Mat Gallien
  • Doors for 47FTH

    What type of doors can be used on the 47FTH enclosures? 47FTH-440 47FTH-840 47FTH-844 47FTH-420 47FTH-240 47FTH-880
    Darby
    last modified by Darby
  • I have the 47605-140

    How should the screw on cover be oriented?
    last modified by Mat Gallien
  • Knockouts on MDU Enclosures

    What are the knockout sizes on the Configuration A and Configuration B MDU style Structured Media Enclosures?   PN 47605-4MG 47605-M42 47605-2MG 47605-M28
    Darby
    last modified by Darby
  • How to purchase the Line Distribution Board separately

    Is there a part number to get just the center Line Distribution Board that is included in the structured media panels such as 47603-24P?
    Darby
    last modified by Darby
  • Universal shelf bracket does not fit in media enclosure

    I just received a structured media enclosure (47605-28N), and a universal shelf bracket (47612-UBK) that I ordered through Amazon.  However, the holes on the bracket do not line up with the holes in the enclosure...
    last modified by Amir Kouchekinia
  • Need help

    I purchased an 11-year old home that has a Leviton structured media system with built in speakers installed in several rooms.    Alas, no instructions or audio equipment were included with the house. ...
    last modified by Scott Kardel
  • Do 110 to RJ45 patch cords fit on Leviton's residential 110 boards?

    Yes they do fit, however, using these to test the boards can sometimes damage the circuits. It requires much more force to pull them off then to put them on. The process of removing the 110 cable can cause the circuit...
    last modified by mikeham
  • Is the 47690-6 Bi-directional?

    Yes, The 47690-6 is bidirectional, all Leviton splitters are bi-directional.
    last modified by zacsmith
  • How do I set the 47611-GTY back to factory default settings?

    Step 1. Unplug the power cable from the router.   Step 2. Plug one end of an ethernet/patch cable into port 1 and the other end of the same cable into port 4.   Step 3. Press and release the uplink button....
    last modified by mikeham
  • Cat 5e Voice and Data Board Numbering

    The Leviton Category 5e Voice and Data board is a common piece in many of our Structured Media Center preconfigured panels.  As shown below, the terminations correspond to ports 2,4,6 on the left, and 1,3,5 on th...
    Darby
    last modified by Darby
  • What sizes do your SMC come in?

    I have a 14" structured media center that was in my house when I moved in. I want to expand my system so Iam going to need more room in my enclosure.Do you offer any other sizes?
    last modified by zacsmith
  • Component placement

    Where do you install the Westell modem in the structured wiring panel box? This is my very first installation ever. I know residential power distribution; this is new horizons for me! I'll be installing an Internet, ...
    last modified by George W. Bailey