• Yale with VRCOP+3,VRP03,VRZP15

    I am trying to install 3 x Yale Z Wave locks. I get one working just fine, any one, as long as it is close to the VRCOP. It is my understanding that the Yale VRP03 and VRZP15 should extend the network so all three lo...
    last modified by David Scott
  • Does the VRP15 support beaming?

    The VRP03 Z-Wave dimmer supports beaming, such as to security locks. However, I need an appliance module (non-dimming). Does the VRP15-1LW support beaming? If not, are there any plans for it to support beaming in the ...
    last modified by randman
  • Lost feedback in my entire network

    I have a 50 node all Leviton Vizia RF network in my home. I also have an HAI omnipro II panel. I set up the network with a RZCPG-BSG remote because I didn't require the remote to manage events. The remote died a year ...
    last modified by Jon Yorkis
  • How to extend Zwave to my Guest House...

    I am trying to get Zwave locks managed in my Home Automation system.  13 Locks but I cannot get Zwave to communicate to my guest house from my primary house.  Is there any outside devices that i can put inli...
    last modified by Technical Geek
  • Controlling Schlage door lock using VRCOP

    I have a VRCOP-1LW as well as the Programmer/remote VRCPG. I have managed to get light dimmers onto the zwave network using these devices and I am also able to control them.   However, can somebody please explai...
    last modified by Pranav Shah
  • VROCP update with Windows 2000

    Does anybody know if you can update the firmware on a VROCP using windows 2000? The only PC I have that has a serial port is running XP, I have been told that a USB to RS232 adaptor will not work.   Thanks in ad...
    last modified by Cameron Lane
  • VRC0P +3 Firmware

    It seems Leviton's website has changed and now the link is gone...  How do I get to the latest VRC0P firmware?
    last modified by Ellery Coffman
  • VRI06-1LZ Help

    I replaced a Lutron DV-603P with a VR106-1LZ and swapped the generic paddle switch on the other end of the three-way with a VP00R-10Z. The lights come on fine and the VR106 allows me to dim them. However, the VP00R wo...
    last modified by dwilkison
  • Vizia RF installation/set up questions

    Greetings and Happy New Years!   I am new to Z-wave and the Vizia RF products so my appoligies if my questions are simple.    zwave products = mainly the RZ106 dimmers in sinlge pull, three way ...
    last modified by Larry Pines
  • Why don’t all of the Vizia Scene controllers show up as controllers on the device list?

    Just completed a Network rediscovery and cannot do the update controller because 4 Scene controllers are not hi-lighted green on the list of devices as are the other scene controllers. The device list shown in the att...
    last modified by bobf
  • LED Holiday lights and Viziz VRR15-1LZ, RZP03-1LW

    1) I have noticed that when using LED Holiday lights with VRR15-1LZ and the RZP03-1LW that they do not turn off completely.  Is this correct?  Can anything be done about this?   2) The VRS15-1LZ works ...
    last modified by PaulB
  • How do It should be done when you have several VRCZ4-1L in the same environment?

    Hello,   I have a problem with VRCZ4-1L. I'm trying to install two units VRCZ4-1L in a room with 10 units zwave dimer, but can set only the first VRCZ4-1L. Apparently I'm doing all the procedures correctly:  ...
  • VRI06-1LZ: Associations help

    Hi folks - Just installed a Leviton VRI06-1LZ. HomeSeer settings all seem correct except no Associations will fire. HomeSeer allows me to create associations and save them, just like I have done successfully wit...
    last modified by James Waid
  • 6400 and 6450-4 controllers HELP!!!!!

    For the life of me please help!!!!! I need a copy of the instruction sheet for "Wall Controller Keyboard Cat. No. 6450-4" & " Wall Controller with Annunciator Cat. No. 6400" I have hours on line trying to find doc...
    last modified by David Kaufman
  • When I select  RS232 Setup the rzcpg-bsg remote gives me "No RS232 DEV"

    Hello, I am following the instrucitons found in the VRC0P_ASCII_Programming_Application_Note.pdf, specifically the steps below.  I am assuming that the instrucitons apply to the RZC0P serial device as well. Whe...
    last modified by patrick beauchemin
  • Interference from LED Lights

    I have GE/Jasco LED undercabinet light banks (2 sets of banks with 3 LEDs each) under one section of our cabinets in the kitchen.  The LED's are wired in series to a double switch (single gang, two loads) with th...
    last modified by gduren
  • Cannot include VRC0P with my RZCPG remote

    Just purchased a VRC0P-1LW to replace my RZC0P serial device.  For the life of me I cant add the VRC0P-1LW as a node.  I have followed the instructions and put the serial device into programming mode but the...
    last modified by patrick beauchemin
  • VRC0P: any way to query device class information by node?

    With VRC0P, is there a way to query what classes (basic, generic, specific) device belongs to?   FI command can search for node(s) matching to specific classes, but it would be very useful to be able to do the l...
    last modified by tjkofi
  • VRC0P +3 firmware bug?

    It would seem like there is bug in VRC0P firmware causing it to "lock up" (go to a loop) if one sends a query to the node number of the VRC0P itself?   This seems to happen atleast with latest firmware: $Leviton...
    last modified by tjkofi
  • VIZIA VRCOP +3 issue with Yale Locks

    Is the new VRCOP 3 compatible with the new Yale Locks?   I have purchased both but am unable to get the lock to respond.  It will include but when I send the lock command found in the VRCOP protocol doc...
    last modified by Ken Goldsberry