• WiFi Dimmer DW6HD - Bulk Firmware Update

    I have over 20 of these light switches in my house, and the firmware update process is extremely cumbersome. It takes ~5 minutes per switch to do a firmware update. So, every time there is a firmware update, I have to...
    last modified by Beau Clark
  • VRCS2-MRZ documentation

    Some functions of the  VRCS2-MRZ are not documented in the papers that ship with the product. For example, when a button on an included device is held down, the led begins flashing green. What does that mean? Als...
    last modified by Don Miller
  • dimmer levels fail to save when programming scene

    I just recently performed a full reset on a vizier rf+ installation.  Everything works except programming scenes.  When programming a scene on any controller (4, 2, or 1 button), the dimmer levels fail to sa...
    last modified by Leon Podolsky
  • ControlThink ThinkEssentials v2.5

    Hi All,   looking to find the final version of ThinkEssentials v2.5 Beta (build2)   ThinkEssentials v2.5 Beta (build2) -- Attached - ControlThink Forums   can NOT find it anywhere online.   i'm...
    last modified by Tal Jack
  • Is there beaming support in switches and dimmers yet?

    Is there a list anywhere of what modules/controllers and Leviton devices support beaming. Older posts go back to April '11, and I'm trying to find out if I'll need to purchase a VRP03-1LW plug in lamp control module i...
    last modified by Jonathan Dunlap
  • Will a VRF01-1LZ Switch Control A Natural Gas Fireplace Fan?

    I have a direct vent, natural gas fireplace.   The internal fireplace fans are controlled via a 115V switch on the wall independent of whether the flame is on or not.   Will a VRF01-1LZ (Scene Capable, Qu...
    last modified by Doug Fraser
  • VR106 Z-wave dimmers and LED bulbs

    I have several VR106 600w z-wave dimmers.  I want to replace the incandescent bulbs with LED's.  I did this in one room with a 3 way switch (remote switch has an led locator light) that powers 4 can lights.&...
    last modified by DNLLB
  • Zwave Controller

    VRCPG-0SG controller works but screen shows no characters is there a fix for this?
    last modified by Russell Cheatham
  • Vizia RF Network Extreme Lag Time

    I have a 37 node system with a combination of door locks, thermostats and lamp modules. The door locks and thermostats worked great using a few lamp modules at "repeaters". I just added 15 lamp dimmers and even though...
    last modified by Randy Garcia
  • ViziaRF+ scene response times

    I have a 46 node ViziaRF+ lighting system installed including 15A switches, 600W dimmers, ELV dimmers and 15A receptacles + some 4-button scene controllers.  The house is only 1500 sq/ft.  When a scene is pr...
    last modified by Kent Oberlin
  • VRCS1 No Local Control, LED's working

    I have a VRCS1 that I'm trying to install to control our outside lights. I have power to the switch as I can get the LED's to function, but toggling the switch does not control the lights? I noticed on the instruction...
    last modified by Chris Straface
  • Help with Kwikset lock

    I need some help with getting a new Kwikset lock to work. I have two other locks which work fine. All controlled with a VRC0P. I can control them from a HAI system or directly using a terminal program on my laptop. Th...
    last modified by SJ Hart
  • Installer Tool V1.1.1.0 Available

    Installer Tool V1.1.1.0 is now available via www.leviton.com/rfinstaller.
  • Leviton 6312 lights light turn on/off only part of the week

    Hi i have a leviton 6312 the light switch that works the exterior lights on my house has a green lit light i have checked the programming and they are set to turn the lights on at 7pm and off at 6am they only do t...
    last modified by stephanie vogt
  • VRC0P+3 Schlage deadbolt support

    I have two Z wave Schlage BE369NX locks. I have added them to the Leviton Z Wave network and ran RS-232 setup successfully.   What are the ASCII command that I can send to the Schlage locks?   The locks a...
    last modified by Eli Yaron
  • VRCS4-MR local load control

    I have a VRCS4-MR that I cannot control the local load. I can hear the relay switch, but there is always line voltage at the switch terminal on the controller. I've attempted a factory reset and still the same results.
    last modified by cpaiged
  • Scene Controller and 3 Way Circuits

    I just moved into  new apt. and am transferrinf my Vizia RF+ gear from my previous home. I have a VRCZ4-MR Scene controller with load control and I want to place this at a location that is a 3-way circuit. I also...
    last modified by Mike Potts
  • pr180 causes light to blink when set to auto

    I installed the PR180 in our kitchen this weekend. The problem is that when set to the auto position the light blinks. It seems to stop after about 5 minutes. This is really annoying. Is this a bad switch?
    last modified by Josh McCann
  • Zones, Areas, Groups, Associaitons

    Can someone provide the "real" definitions and differences for the Z-Wave Terms: Zones Areas Groups Associaitons Seems like these terms are often trhown around and few people know what they really are.   In...
    last modified by jwilleke
  • Having trouble with VRCS2

    Hi, I am having trouble configuring the VRCS2 double control. I follow the programming procedure in order to include it into the remote control VRCPG following the regular procedure: 1. Pressing both buttons in order...
    last modified by Roberto Cadena