<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:clearspace="http://www.jivesoftware.com/xmlns/clearspace/rss" xmlns:dc="http://purl.org/dc/elements/1.1/" version="2.0">
  <channel>
    <title>Leviton Online Knowledgebase: Message List - What is the difference between the 69586-UXX and the 69270-UXX patch panels?</title>
    <link>http://communities.leviton.com/community/knowledgebaseforums/network_solutions/products/copper/patch_panels?view=discussions</link>
    <description>Most recent forum messages</description>
    <language>en</language>
    <pubDate>Fri, 25 Mar 2011 15:58:26 GMT</pubDate>
    <generator>Jive SBS 4.5.5.2  (http://jivesoftware.com/products/clearspace/)</generator>
    <dc:date>2011-03-25T15:58:26Z</dc:date>
    <dc:language>en</dc:language>
    <item>
      <title>What is the difference between the 69586-UXX and the 69270-UXX patch panels?</title>
      <link>http://communities.leviton.com/message/2533?tstart=0#2533</link>
      <description>&lt;!-- [DocumentBodyStart:5e52358f-3cc6-4a9e-8854-89a94ddb9980] --&gt;&lt;div class="jive-rendered-content"&gt;&lt;p&gt;Both of these patch panels are Cat 6 rated, and offer the same performance qualities.&amp;#160; The difference is in the configuration of the ports:&lt;/p&gt;&lt;p style="min-height: 8pt; height: 8pt; padding: 0px;"&gt;&amp;#160;&lt;/p&gt;&lt;p&gt;The 69270 series comes with individual Cat 5e+ jacks that are meant to be terminated and then snapped in to the panel.&lt;/p&gt;&lt;p style="min-height: 8pt; height: 8pt; padding: 0px;"&gt;&amp;#160;&lt;/p&gt;&lt;p&gt;The 69586 series comes with the ports pre-loaded in groupings of 6, and the punchdown is done directly on the panel. &lt;/p&gt;&lt;p style="min-height: 8pt; height: 8pt; padding: 0px;"&gt;&amp;#160;&lt;/p&gt;&lt;p&gt;Pratcically speaking, with the 69586, if there is an issue with a single port (i.e. it gets damaged during installation) you must remove the entire group of 6 jacks to replace it.&amp;#160; However the installation may be faster as you do not need to snap in each jack individually. With the 69270, if a port needs to be replaced, it is just a matter of snapping in a single new jack.&lt;/p&gt;&lt;/div&gt;&lt;!-- [DocumentBodyEnd:5e52358f-3cc6-4a9e-8854-89a94ddb9980] --&gt;</description>
      <pubDate>Fri, 25 Mar 2011 15:58:26 GMT</pubDate>
      <author>CommunityAdmin@leviton.com</author>
      <guid>http://communities.leviton.com/message/2533?tstart=0#2533</guid>
      <dc:date>2011-03-25T15:58:26Z</dc:date>
      <clearspace:dateToText>2 years, 1 month ago</clearspace:dateToText>
      <clearspace:objectType>0</clearspace:objectType>
    </item>
  </channel>
</rss>